how can i get rtsps server sourcecode of asc8851a

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how can i get rtsps server sourcecode of asc8851a

1,408 Views
steven03lee
Contributor I

anyone can give me the SDK of asc8851a, mine is 6.1.1, but the rtsps doesnot work well.

help,please

0 Kudos
Reply
3 Replies

1,235 Views
Carlos_Musich
NXP Employee
NXP Employee

Hi Steven,

the rtsps server and the asc8851a are independent. I assume you are using an i.MX processor with it. If you are generating the i.MX image with Yocto you can use bitbake -s │ gerp rtsps command to find the Yocto package you may need to include this service.

If you are not using i.MX processor please let me know.


Regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,235 Views
steven03lee
Contributor I

Hi Carlos,

   I'm now using NXP ASC8851AET(not i.MX), and looking for the SDK.

we have used asc8851a for years,recently we found the rtsp server in the sdk doesnot work well, so i want to know is there a new sdk or rtsp server can fix it.

thanks for your reply

0 Kudos
Reply

1,235 Views
Carlos_Musich
NXP Employee
NXP Employee

Hi steven,

con you point me please to the link where you download sdk?

0 Kudos
Reply