how can i capture 752 data each row,is there any limit of the max width of a picture

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

how can i capture 752 data each row,is there any limit of the max width of a picture

937 次查看
zhangyanan
Contributor I

i use  i.MX6Q to capture  8-bit Bayer data from a camera, the desired width of a picture is 752, but there is only about 720 data captured in each row, is there any limit of the max width of a picture? how can i capture 752 data in each row?

i am looking forward to your reply

标签 (1)
0 项奖励
回复
1 回复

896 次查看
igorpadykov
NXP Employee
NXP Employee

Hi zhang

please check frame size settings using sect.37.5.152 CSI0 Sense Frame Size Register

(IPUx_CSI0_SENS_FRM_SIZE) i.MX6DQ Reference Manual

http://www.nxp.com/docs/en/reference-manual/IMX6DQRM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复