how can i capture 752 data each row,is there any limit of the max width of a picture

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how can i capture 752 data each row,is there any limit of the max width of a picture

970 Views
zhangyanan
Contributor I

i use  i.MX6Q to capture  8-bit Bayer data from a camera, the desired width of a picture is 752, but there is only about 720 data captured in each row, is there any limit of the max width of a picture? how can i capture 752 data in each row?

i am looking forward to your reply

Labels (1)
0 Kudos
Reply
1 Reply

929 Views
igorpadykov
NXP Employee
NXP Employee

Hi zhang

please check frame size settings using sect.37.5.152 CSI0 Sense Frame Size Register

(IPUx_CSI0_SENS_FRM_SIZE) i.MX6DQ Reference Manual

http://www.nxp.com/docs/en/reference-manual/IMX6DQRM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply