help

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

help

1,489件の閲覧回数
zhangbaobing
Contributor II

The problem of IMX6 POWERED OFF will generate to TF card reading and writing failure .

And then, are there some solutions to solve this question?

as followings :

supercapacitors 

powerd off delay 

OR the others to offer us .

thanks all

ラベル(1)
0 件の賞賛
返信
1 返信

1,452件の閲覧回数
b36401
NXP Employee
NXP Employee

Please make sure that the board meats power-off sequence.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信