hdmi without ddc or i2c

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

hdmi without ddc or i2c

2,163 次查看
xiaojun_huang
Contributor I

Hello, I'm work with imx6q custon board.

We made changes on Android O, using HDMI as the display output.

But we are not connected to I2C or DDC to HDMI, only TMDS and CLOCK, and there is no HPD signal and CEC signal.
We hope to force the output of the HDMI signal. What should we do?
I look forward to hearing from you.

标签 (1)
标记 (1)
0 项奖励
回复
2 回复数

1,894 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Jun

one can look at tutorial from boundary devices

DVI Support on i.MX6 boards - Boundary Devices 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,894 次查看
xiaojun_huang
Contributor I

Thanks for your replay.

This patch uses HDMI_DVI_IH_STAT instead of HPD detection,

but I hope that the TMDS signal can be forced out without interrupt method.

Is this feasible?
How should I modify it?

0 项奖励
回复