hdmi without ddc or i2c

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

hdmi without ddc or i2c

2,189 Views
xiaojun_huang
Contributor I

Hello, I'm work with imx6q custon board.

We made changes on Android O, using HDMI as the display output.

But we are not connected to I2C or DDC to HDMI, only TMDS and CLOCK, and there is no HPD signal and CEC signal.
We hope to force the output of the HDMI signal. What should we do?
I look forward to hearing from you.

Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

1,920 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jun

one can look at tutorial from boundary devices

DVI Support on i.MX6 boards - Boundary Devices 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,920 Views
xiaojun_huang
Contributor I

Thanks for your replay.

This patch uses HDMI_DVI_IH_STAT instead of HPD detection,

but I hope that the TMDS signal can be forced out without interrupt method.

Is this feasible?
How should I modify it?

0 Kudos
Reply