hdmi cable connection not detected

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

hdmi cable connection not detected

4,301 Views
angelo_d
Senior Contributor I

Hi,

using imx6q and linux 3.10.17 (boundary).

On hdmi cable connection / disconneciton, no udev event is fired.

bash-3.2# udevadm monitor

monitor will print the received events for:

UDEV - the event which udev sends out after rule processing

KERNEL - the kernel uevent

I am suspecting a possible hw issue

bash-3.2# /lib/systemd/systemd-udevd

systemd-udevd[829]: starting version 208

Every help is appreciated

Thanks

angelo

Labels (2)
0 Kudos
Reply
4 Replies

3,387 Views
angelo_d
Senior Contributor I

Hi Igor, many thanks

i read that thread, but schematic of our board, for the hdmi part, is like sabreauto, so there is a voltage level shifter / protector between cpu and hdmi connector.

Boundary seems have added a patch using RXSENSE pin to detect hdmi monitors, since they had issues with hdmi hotplug detect pin. So the hdmi lcd works at cable connection, but there is not udev event generated.

So in my case, seems an hw problem, with the circuit adjusted differently, the hotplug detection start to work.

0 Kudos
Reply

3,387 Views
zhanghaijian
Contributor II

Hi angelo

I have the same problem as you,if you can ,tell me how to do ,thanks.

0 Kudos
Reply

3,387 Views
angelo_d
Senior Contributor I

Seems i have some issues with the hot-plug detect pin.

Without any cable connected it is at 1V. With cable connected reach 2,24V, so there seems to be some pinmux configuration issue.

Strangely, in don't find this pin in the pinmux config map.

0 Kudos
Reply

3,387 Views
igorpadykov
NXP Employee
NXP Employee

Hi angelo

one can check post on boundarydevices forum with similar issue

RooT

June 27, 2013 at 10:35 am..

http://boundarydevices.com/i-mx6-kernel-l3-0-35_4-0-0/

Best regards

igor

0 Kudos
Reply