hardware based video decoder example for freescale i-max6 dual processor.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

hardware based video decoder example for freescale i-max6 dual processor.

1,766 Views
sarfrazahmed07
Contributor I

I need a working example for hardware based video decoder for MJPG stream for i-max6 dual processor. Thanks

Tags (4)
1 Reply

1,513 Views
igorpadykov
NXP Employee
NXP Employee

Hi Safraz

one can use gplay or imx-test package included in ltib (mxc_vpu_test):

./mxc_vpu_test.out -D "-i /usr/vectors/file.mjpg -f 7"

Note that mxc_vpu_test can only play RAW video files.

Also next link may be useful

JPEG hardware decode and resize in i.MX6

Best regards

igor