hardware acceleration supporting of directfb in directfb v1.6 in yocto "dylan"

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

hardware acceleration supporting of directfb in directfb v1.6 in yocto "dylan"

Jump to solution
2,269 Views
jojorong
Contributor IV

Hi,

     because of the hardware acceleration of directfb with version 1.4.0 is not match with in dylan (v1.6.1),

     

     so, there is someone is supporting(developing) this to make it's valid also in dylan ?

Labels (3)
1 Solution
1,464 Views
daiane_angolini
NXP Employee
NXP Employee

I think you were already replied in meta-freescale :smileywink:

Just in case other people are looking for this:

https://lists.yoctoproject.org/pipermail/meta-freescale/2013-May/002685.html

View solution in original post

3 Replies
1,465 Views
daiane_angolini
NXP Employee
NXP Employee

I think you were already replied in meta-freescale :smileywink:

Just in case other people are looking for this:

https://lists.yoctoproject.org/pipermail/meta-freescale/2013-May/002685.html

1,464 Views
jojorong
Contributor IV

Hi,

But …. unfortunate, maybe there is a bug about for HW acceleration of DirectFB v1.4.0 about for "can not display cursor when moving to HW accelerated DirectFB "

It's normal to display cursor when i disable HW acceleration of DirecFB,

in the HW acceleration case, when i move the cursor to the DFB surface,

it disappear (it looks like the surface is top on the cursor).

It''s a bug ? Maybe cursor need to be HW accelerated also ?

I use the GTK+(v2.24.15) top on DirectFB(v1.4.0).

Thanks,

- Jojo

在 2013年5月16日星期四,上午2:17,Daiane Angolini 写道:

hardware acceleration supporting of directfb in directfb v1.6 in yocto "dylan"

created by Daiane Angolini (https://community.freescale.com/people/DaianeAngolini) in i.MX Community - View the full discussion (https://community.freescale.com/message/329526#329526)

I think you were already replied in meta-freescale :smileywink:

Reply to this message by replying to this email -or- go to the message on Freescale Community (https://community.freescale.com/message/329526#329526)

Start a new discussion in i.MX Community by email (mailto:discussions-community-imx@freescale-phx.hosted.jivesoftware.com ) or at Freescale Community (https://community.freescale.com/choose-container.jspa?contentType=1&containerType=14&container=2004)

>

0 Kudos
Reply
1,464 Views
daiane_angolini
NXP Employee
NXP Employee

I´m sorry, I don´t know what´s the expected behavior for DirectFB.

I hope someone else in community knows

0 Kudos
Reply