hardknott-5.10 build failure for isp-imx_4.2.2.13.0 - files not found during cp

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

hardknott-5.10 build failure for isp-imx_4.2.2.13.0 - files not found during cp

1,260 Views
ptoth
Contributor I

I am receiving an error when running bitbake to build a yocto hardknott 5.10 image for my Variscite imx8mp

This line in isp-imx_4.2.2.13.0.bb:

    cp -r ${WORKDIR}/build/generated/release/bin/*2775* ${D}/opt/imx8-isp/bin

Does not find any files matching the name "*2775*" and errors out.

Can anyone provide some help? I have no idea where to look to solve this.

Full error messages:

ERROR: isp-imx-4.2.2.13.0-r0 do_install: ExecutionError('/workdir/build_xwayland/tmp/work/cortexa53-crypto-mx8mp-fslc-linux/isp-imx/4.2.2.13.0-r0/temp/run.do_install.1064809', 1, None, None)
ERROR: Logfile of failure stored in: /workdir/build_xwayland/tmp/work/cortexa53-crypto-mx8mp-fslc-linux/isp-imx/4.2.2.13.0-r0/temp/log.do_install.1064809
Log data follows:
| DEBUG: Executing python function extend_recipe_sysroot
| NOTE: Direct dependencies are ['/workdir/sources/meta-freescale/recipes-graphics/imx-gpu-g2d/imx-gpu-g2d_6.4.3.p2.0.bb:do_populate_sysroot', '/workdir/sources/poky/meta/recipes-devtools/quilt/quilt-native_0.66.bb:do_populate_sysroot', '/workdir/sources/poky/meta/recipes-devtools/gcc/gcc-cross_10.3.bb:do_populate_sysroot', '/workdir/sources/meta-freescale/recipes-kernel/linux/linux-imx-headers_5.10.bb:do_populate_sysroot', 'virtual:native:/workdir/sources/poky/meta/recipes-devtools/pseudo/pseudo_git.bb:do_populate_sysroot', '/workdir/sources/poky/meta/recipes-devtools/python/python3_3.9.9.bb:do_populate_sysroot', '/workdir/sources/poky/meta/recipes-devtools/gcc/gcc-runtime_10.3.bb:do_populate_sysroot', '/workdir/sources/poky/meta/recipes-core/systemd/systemd-systemctl-native.bb:do_populate_sysroot', '/workdir/sources/poky/meta/recipes-devtools/cmake/cmake-native_3.19.5.bb:do_populate_sysroot', 'virtual:native:/workdir/sources/poky/meta/recipes-devtools/patch/patch_2.7.6.bb:do_populate_sysroot', '/workdir/sources/meta-freescale/recipes-graphics/drm/libdrm_2.4.102.imx.bb:do_populate_sysroot', '/workdir/sources/poky/meta/recipes-core/glibc/glibc_2.33.bb:do_populate_sysroot']
| NOTE: Installed into sysroot: []
| NOTE: Skipping as already exists in sysroot: ['imx-gpu-g2d', 'quilt-native', 'gcc-cross-aarch64', 'linux-imx-headers', 'pseudo-native', 'python3', 'gcc-runtime', 'systemd-systemctl-native', 'cmake-native', 'patch-native', 'libdrm', 'glibc', 'imx-gpu-viv', 'gmp-native', 'linux-libc-headers', 'binutils-cross-aarch64', 'gnu-config-native', 'xz-native', 'libmpc-native', 'texinfo-dummy-native', 'libtool-native', 'automake-native', 'autoconf-native', 'zlib-native', 'flex-native', 'mpfr-native', 'libnsl2', 'bzip2', 'zlib', 'util-linux', 'opkg-utils', 'sqlite3', 'libtirpc', 'gdbm', 'libffi', 'openssl', 'libxcrypt', 'readline', 'xz', 'libgcc', 'ncurses-native', 'curl-native', 'bzip2-native', 'attr-native', 'libpthread-stubs', 'libpciaccess', 'libxshmfence', 'wayland', 'libxcb', 'mesa', 'libxxf86vm', 'gettext-minimal-native', 'm4-native', 'libcap-ng', 'ncurses', 'util-linux-libuuid', 'bash-completion', 'libpam', 'pkgconfig-native', 'openssl-native', 'util-macros', 'libx11', 'expat', 'libxml2', 'xorgproto', 'libxau', 'xcb-proto', 'libxdmcp', 'xrandr', 'wayland-protocols', 'libxfixes', 'libxdamage', 'libxext', 'cracklib', 'flex', 'xtrans', 'libxrandr', 'libxrender']
| DEBUG: Python function extend_recipe_sysroot finished
| DEBUG: Executing shell function do_install
| cp: cannot stat '/workdir/build_xwayland/tmp/work/cortexa53-crypto-mx8mp-fslc-linux/isp-imx/4.2.2.13.0-r0/build/generated/release/bin/*2775*': No such file or directory
| WARNING: /workdir/build_xwayland/tmp/work/cortexa53-crypto-mx8mp-fslc-linux/isp-imx/4.2.2.13.0-r0/temp/run.do_install.1064809:155 exit 1 from 'cp -r /workdir/build_xwayland/tmp/work/cortexa53-crypto-mx8mp-fslc-linux/isp-imx/4.2.2.13.0-r0/build/generated/release/bin/*2775* /workdir/build_xwayland/tmp/work/cortexa53-crypto-mx8mp-fslc-linux/isp-imx/4.2.2.13.0-r0/image/opt/imx8-isp/bin'
| WARNING: Backtrace (BB generated script):
| #1: do_install, /workdir/build_xwayland/tmp/work/cortexa53-crypto-mx8mp-fslc-linux/isp-imx/4.2.2.13.0-r0/temp/run.do_install.1064809, line 155
| #2: main, /workdir/build_xwayland/tmp/work/cortexa53-crypto-mx8mp-fslc-linux/isp-imx/4.2.2.13.0-r0/temp/run.do_install.1064809, line 175
| ERROR: ExecutionError('/workdir/build_xwayland/tmp/work/cortexa53-crypto-mx8mp-fslc-linux/isp-imx/4.2.2.13.0-r0/temp/run.do_install.1064809', 1, None, None)
ERROR: Task (/workdir/sources/meta-freescale/recipes-bsp/isp-imx/isp-imx_4.2.2.13.0.bb:do_install) failed with exit code '1'

  

0 Kudos
Reply
1 Reply

1,223 Views
AldoG
NXP TechSupport
NXP TechSupport

Hello,

Since you are using a Variscite Board, and most probably their BSP, I think it may be better to ask in their customer portal.
https://variwiki.com/index.php?title=Customer_Portal

Anyways, did you follow the steps to build the image from their guides?
Which image are you trying to build?

Best regards,
Aldo.

0 Kudos
Reply