gui

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

gui

1,698 Views
sreekanthpk
Contributor I

hi,

  I used bitbake core-image-x11 -c populate_sdk and the bit bake is finished without any error. While I am trying to copy the image to sd card  I can not found the .sdcard file.Is it different  from the normal bit bake command bitbake core-image-base.?Where I can find the .sdcard file?what is the further step I have to proceed? Is bitbake core-image-x11 is not a valid command?Can any body help me to solve this? Please give  some link

Labels (1)
0 Kudos
Reply
1 Reply

1,606 Views
Yuri
NXP Employee
NXP Employee

Hello,

"After a build is complete, the created image resides in <build directory>/tmp/deploy/images."

  Also, please look at Guide to the .sdcard format


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply