gstreamer error imx28

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

gstreamer error imx28

960件の閲覧回数
tip
Contributor I

Hi

I am using a TX28 som from karo (imx287 onboard).

I am using BSP from KARO - based on 3.2 kernel together with ltib (freescale codec enabled)

I have tried gplay on the imx28 eval board with succes - i.e. i can play an mp4 and show on the tft display - but on my custom made board with TX28 i have some trouble in playing video.

Things i know works:

1) frambuffer can show a pic. with fbv  = works

2) gst-launch videotestsrc ! fbdevsink  => works 

3) gst-launch audiotestsrc ¡ alsasink => works

4) gplay carl.mp4 => works on imx. eval board - but not on my custom made board.

I am pretty sure that it's not a hardware issue but a sw issue releated to ltib and my bsp 3.2 kernel

I have embedded a log file when i am running "gplay carl.mp4" (audio works - but nothing is show on the tft display (fb0) - everything seems to work and after 1.38 minutes gplayer stops as it should.

My frame buffer is not blanked - i can show a picture with fbv with succes.

I can neither figure out  the assert error:

(<unknown>:1158): GStreamer-CRITICAL **: gst_caps_ref: assertion `GST_CAPS_REFCOUNT_VALUE (caps) > 0' failed

I think i have read something about gst_v4lsink using fb2 ?

Can it be an overlay problem?

any suggestion is very much appreciated.

-peter

ラベル(1)
タグ(2)
0 件の賞賛
返信
0 返答(返信)