gstreamer display embedded subtitles

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

gstreamer display embedded subtitles

4,621 Views
lachezarnikolov
Contributor I

Hello,

I have a file with embedded subtitles and I am trying to display them along with the picture. The file is an .mkv file with one video, one audio and three subtitle streams. Here's what vlc says about the file:

tales_from_earthsea_codec_info.png

When I play the stream on my linux box using

gst-launch-0.10 filesrc location = /mnt/hgfs/work/test_videos/Tales.from.Earthsea\[h264.dts\]\[niizk\].mkv ! decodebin2 name=dec ! subtitleoverlay name=overlay ! ffmpegcolorspace ! autovideosink  dec. ! overlay.

everything works correctly. However when I try to play that on the i.MX6 board using

gst-launch-0.10 filesrc location = /mnt/sdb1/kur/Tales.from.Earthsea\[h264.dts\]\[niizk\].mkv ! decodebin2 name=dec ! subtitleoverlay name=overlay ! ffmpegcolorspace ! mfw_v4lsink  dec. ! overlay.

it plays the video fine but it doesn't display any subtitles. The output is:

MFW_GST_V4LSINK_PLUGIN 3.0.5 build on Oct 22 2013 15:33:00.

Setting pipeline to PAUSED ...

Pipeline is PREROLLING ...

Aiur: 3.0.5

Core: MKVPARSER_01.04.01  build on Dec 10 2012 15:43:34

  mime: video/x-matroska ; video/webm

  file: /usr/lib/imx-mm/parser/lib_mkv_parser_arm11_elinux.so

Content Info:

  URI:

       file:///mnt/sdb1/kur/Tales.from.Earthsea[h264.dts][niizk].mkv

  Idx File:

       /root/.aiur/.mnt.sdb1.kur.Tales.from.Earthsea[h264.dts][niizk].mkv.aidx

  Seekable  : Yes

  Size(byte): 2100598489

Movie Info:

  Seekable  : Yes

  Live      : No

  Duration  : 1:55:29.856000000

  ReadMode  : Track

  Track     : 5

Track 00 [video_000000] Enabled

  Duration: 1:55:29.856000000

  Language: und

  Mime:

       video/x-h264, parsed=(boolean)true, width=(int)656, height=(int)432, framerate=(

       fraction)23/1, codec_data=(buffer)0000000167640033ac34e380a437a1000003007d000017

       6a8f18318e800000000168eebce5531cc305d2628d13080214868783a1c0d04e12142c0ac0da02fe

       10042ad35e9e850b748c778a1410088b172105449ca3050e204448b20a4d8a081827090809848541

       dc4290a43164215a201900cae8340f81e86f03300b6017002ac05981d61a07802a8400a902087404

       700bc010506e036404b811805902e07203e0087ff85b

vpudec versions :smileyhappy:

  plugin: 3.0.5

  wrapper: 1.0.28(VPUWRAPPER_ARM_LINUX Build on Oct 22 2013 15:28:56)

  vpulib: 5.4.10

  firmware: 2.1.8.34588

Track 01 [audio_000000] Enabled

  Duration: 1:55:29.856000000

  Language: jpn

  Mime:

       audio/x-dts, channels=(int)6, rate=(int)48000, bitrate=(int)0

Track 02 [subtitle]: Disabled

  Codec: 6, SubCodec: 0

Track 03 [subtitle]: Disabled

  Codec: 7, SubCodec: 0

Track 04 [subtitle]: Disabled

  Codec: 7, SubCodec: 0

>>V4L_SINK: Actually buffer status:

  hardware buffer : 21

  software buffer : 0

Pipeline is PREROLLED ...

Setting pipeline to PLAYING ...

full screen size:800x480

[V4L Update Display]: left=0, top=0, width=800, height=480

New clock: GstSystemClock

As you can see aiurdemux reports that the subtitle tracks are disabled. Do you have any Idea how I can make this work?

Please tell me if you need some additional info.

Labels (1)
Tags (3)
0 Kudos
Reply
3 Replies

3,086 Views
YixingKong
Senior Contributor IV

Lachezar

This discussion is closed since no activity. If you still need help, please feel free to reply with an update to this discussion, or create another discussion.

Thanks,

0 Kudos
Reply

3,086 Views
YixingKong
Senior Contributor IV

Lachezar

We have not got your response yet and will close the discussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.

Thanks,

Yixing

0 Kudos
Reply

3,086 Views
YixingKong
Senior Contributor IV

Lachezar


We are sorry for getting back to you so late. Are you still stuck with the issue? If you have somehow to resolved the issue, can we close the discussion? If you still need help, please feel free to reply with an update to this discussion.

Thanks,
Yixing

0 Kudos
Reply