gst-fsl-plugins build failure

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

gst-fsl-plugins build failure

跳至解决方案
1,765 次查看
ketandeshpande
Contributor I

Hello Everybody,

        I am trying to compile the latest LTIB L3.0.35_4.1.0_130816_source.tar.gz and everything works fine till I reach the gst-fsl-plugins build. As I can see, the compilation is also not throwing any error. The plugin configuration itself seems failing. Can somebody tell me what am I doing wrong? or What is it that I am missing?

        Below is the log I get when I try to compile ltib using './ltib'

Processing: gst-fsl-plugins

=============================

Build path taken because: directory build, build key set, no prebuilt rpm,

rpmbuild --dbpath /home/jci/ltib_test/ltib/rootfs//var/lib/rpm --target arm --define '_unpackaged_files_terminate_build 0' --define '_target_cpu arm' --define '__strip strip' --define '_topdir /home/jci/ltib_test/ltib/rpm' --define '_prefix /usr' --define '_tmppath /home/jci/ltib_test/ltib/tmp' --define '_rpmdir /home/jci/ltib_test/ltib/rpm/RPMS'  --define '_mandir /usr/share/man' --define '_sysconfdir /etc' --define '_localstatedir /var' -bc --short-circuit  /home/jci/ltib_test/ltib/dist/lfs-5.1/fsl-mm/gst-fsl-plugins.spec

Building target platforms: arm

Building for target arm

Executing(%build): /bin/sh -e /home/jci/ltib_test/ltib/tmp/rpm-tmp.25237

+ umask 022

+ cd /home/jci/ltib_test/ltib/rpm/BUILD

+ cd gst-fsl-plugins-3.0.7

++ which pkg-config

+ export 'PKG_CONFIG=/opt/freescale/ltib/usr/bin/pkg-config --static '

+ PKG_CONFIG='/opt/freescale/ltib/usr/bin/pkg-config --static '

++ sed 's,imx\([0-9]*\).*,MX\1,g'

++ echo imx6q

+ PLATFORMSHORTNAME=MX6

+ '[' xMX6 = xMX27 ']'

+ export FBHEADER_PATH=/home/jci/ltib_test/ltib/rootfs/usr/src/linux/include/

+ FBHEADER_PATH=/home/jci/ltib_test/ltib/rootfs/usr/src/linux/include/

++ sed 's,imx\([0-9]*\).*,MX\1,g'

++ echo imx6q

+ ./autogen.sh PLATFORM=MX6

+ aclocal

+ libtoolize --force

libtoolize: putting auxiliary files in `.'.

libtoolize: linking file `./ltmain.sh'

libtoolize: putting macros in AC_CONFIG_MACRO_DIR, `m4'.

libtoolize: linking file `m4/libtool.m4'

libtoolize: linking file `m4/ltoptions.m4'

libtoolize: linking file `m4/ltsugar.m4'

libtoolize: linking file `m4/ltversion.m4'

libtoolize: linking file `m4/lt~obsolete.m4'

+ automake -a

libs/Makefile.am:1: Libtool library used but `LIBTOOL' is undefined

libs/Makefile.am:1:   The usual way to define `LIBTOOL' is to add `AC_PROG_LIBTOOL'

libs/Makefile.am:1:   to `configure.ac' and run `aclocal' and `autoconf' again.

libs/Makefile.am:1:   If `AC_PROG_LIBTOOL' is in `configure.ac', make sure

libs/Makefile.am:1:   its definition is in aclocal's search path.

src/audio/aac_dec/src/Makefile.am:16: Libtool library used but `LIBTOOL' is undefined

src/audio/aac_dec/src/Makefile.am:16:   The usual way to define `LIBTOOL' is to add `AC_PROG_LIBTOOL'

src/audio/aac_dec/src/Makefile.am:16:   to `configure.ac' and run `aclocal' and `autoconf' again.

src/audio/aac_dec/src/Makefile.am:16:   If `AC_PROG_LIBTOOL' is in `configure.ac', make sure

src/audio/aac_dec/src/Makefile.am:16:   its definition is in aclocal's search path.

src/audio/aacplus_dec/src/Makefile.am:29: Libtool library used but `LIBTOOL' is undefined

src/audio/aacplus_dec/src/Makefile.am:29:   The usual way to define `LIBTOOL' is to add `AC_PROG_LIBTOOL'

src/audio/aacplus_dec/src/Makefile.am:29:   to `configure.ac' and run `aclocal' and `autoconf' again.

src/audio/aacplus_dec/src/Makefile.am:29:   If `AC_PROG_LIBTOOL' is in `configure.ac', make sure

src/audio/aacplus_dec/src/Makefile.am:29:   its definition is in aclocal's search path.

src/audio/ac3_dec/src/Makefile.am:4: Libtool library used but `LIBTOOL' is undefined

src/audio/ac3_dec/src/Makefile.am:4:   The usual way to define `LIBTOOL' is to add `AC_PROG_LIBTOOL'

src/audio/ac3_dec/src/Makefile.am:4:   to `configure.ac' and run `aclocal' and `autoconf' again.

src/audio/ac3_dec/src/Makefile.am:4:   If `AC_PROG_LIBTOOL' is in `configure.ac', make sure

src/audio/ac3_dec/src/Makefile.am:4:   its definition is in aclocal's search path.

src/audio/amr_dec/src/Makefile.am:13: Libtool library used but `LIBTOOL' is undefined

src/audio/amr_dec/src/Makefile.am:13:   The usual way to define `LIBTOOL' is to add `AC_PROG_LIBTOOL'

src/audio/amr_dec/src/Makefile.am:13:   to `configure.ac' and run `aclocal' and `autoconf' again.

src/audio/amr_dec/src/Makefile.am:13:   If `AC_PROG_LIBTOOL' is in `configure.ac', make sure

src/audio/amr_dec/src/Makefile.am:13:   its definition is in aclocal's search path.

src/audio/amr_enc/src/Makefile.am:13: Libtool library used but `LIBTOOL' is undefined

src/audio/amr_enc/src/Makefile.am:13:   The usual way to define `LIBTOOL' is to add `AC_PROG_LIBTOOL'

src/audio/amr_enc/src/Makefile.am:13:   to `configure.ac' and run `aclocal' and `autoconf' again.

src/audio/amr_enc/src/Makefile.am:13:   If `AC_PROG_LIBTOOL' is in `configure.ac', make sure

src/audio/amr_enc/src/Makefile.am:13:   its definition is in aclocal's search path.

src/audio/audio_pp/src/Makefile.am:1: Libtool library used but `LIBTOOL' is undefined

src/audio/audio_pp/src/Makefile.am:1:   The usual way to define `LIBTOOL' is to add `AC_PROG_LIBTOOL'

src/audio/audio_pp/src/Makefile.am:1:   to `configure.ac' and run `aclocal' and `autoconf' again.

src/audio/audio_pp/src/Makefile.am:1:   If `AC_PROG_LIBTOOL' is in `configure.ac', make sure

src/audio/audio_pp/src/Makefile.am:1:   its definition is in aclocal's search path.

src/audio/beep/src/Makefile.am:2: Libtool library used but `LIBTOOL' is undefined

src/audio/beep/src/Makefile.am:2:   The usual way to define `LIBTOOL' is to add `AC_PROG_LIBTOOL'

src/audio/beep/src/Makefile.am:2:   to `configure.ac' and run `aclocal' and `autoconf' again.

src/audio/beep/src/Makefile.am:2:   If `AC_PROG_LIBTOOL' is in `configure.ac', make sure

src/audio/beep/src/Makefile.am:2:   its definition is in aclocal's search path.

src/audio/down_mix/src/Makefile.am:1: Libtool library used but `LIBTOOL' is undefined

src/audio/down_mix/src/Makefile.am:1:   The usual way to define `LIBTOOL' is to add `AC_PROG_LIBTOOL'

src/audio/down_mix/src/Makefile.am:1:   to `configure.ac' and run `aclocal' and `autoconf' again.

src/audio/down_mix/src/Makefile.am:1:   If `AC_PROG_LIBTOOL' is in `configure.ac', make sure

src/audio/down_mix/src/Makefile.am:1:   its definition is in aclocal's search path.

src/audio/mp3_dec/src/Makefile.am:20: Libtool library used but `LIBTOOL' is undefined

src/audio/mp3_dec/src/Makefile.am:20:   The usual way to define `LIBTOOL' is to add `AC_PROG_LIBTOOL'

src/audio/mp3_dec/src/Makefile.am:20:   to `configure.ac' and run `aclocal' and `autoconf' again.

src/audio/mp3_dec/src/Makefile.am:20:   If `AC_PROG_LIBTOOL' is in `configure.ac', make sure

src/audio/mp3_dec/src/Makefile.am:20:   its definition is in aclocal's search path.

src/audio/mp3_enc/src/Makefile.am:19: Libtool library used but `LIBTOOL' is undefined

src/audio/mp3_enc/src/Makefile.am:19:   The usual way to define `LIBTOOL' is to add `AC_PROG_LIBTOOL'

src/audio/mp3_enc/src/Makefile.am:19:   to `configure.ac' and run `aclocal' and `autoconf' again.

src/audio/mp3_enc/src/Makefile.am:19:   If `AC_PROG_LIBTOOL' is in `configure.ac', make sure

src/audio/mp3_enc/src/Makefile.am:19:   its definition is in aclocal's search path.

src/audio/spdif_rx/src/Makefile.am:1: Libtool library used but `LIBTOOL' is undefined

src/audio/spdif_rx/src/Makefile.am:1:   The usual way to define `LIBTOOL' is to add `AC_PROG_LIBTOOL'

src/audio/spdif_rx/src/Makefile.am:1:   to `configure.ac' and run `aclocal' and `autoconf' again.

src/audio/spdif_rx/src/Makefile.am:1:   If `AC_PROG_LIBTOOL' is in `configure.ac', make sure

src/audio/spdif_rx/src/Makefile.am:1:   its definition is in aclocal's search path.

src/audio/spdif_tx/src/Makefile.am:1: Libtool library used but `LIBTOOL' is undefined

src/audio/spdif_tx/src/Makefile.am:1:   The usual way to define `LIBTOOL' is to add `AC_PROG_LIBTOOL'

src/audio/spdif_tx/src/Makefile.am:1:   to `configure.ac' and run `aclocal' and `autoconf' again.

src/audio/spdif_tx/src/Makefile.am:1:   If `AC_PROG_LIBTOOL' is in `configure.ac', make sure

src/audio/spdif_tx/src/Makefile.am:1:   its definition is in aclocal's search path.

src/audio/vorbis_dec/src/Makefile.am:4: Libtool library used but `LIBTOOL' is undefined

src/audio/vorbis_dec/src/Makefile.am:4:   The usual way to define `LIBTOOL' is to add `AC_PROG_LIBTOOL'

src/audio/vorbis_dec/src/Makefile.am:4:   to `configure.ac' and run `aclocal' and `autoconf' again.

src/audio/vorbis_dec/src/Makefile.am:4:   If `AC_PROG_LIBTOOL' is in `configure.ac', make sure

src/audio/vorbis_dec/src/Makefile.am:4:   its definition is in aclocal's search path.

src/audio/wma10_dec/src/Makefile.am:19: Libtool library used but `LIBTOOL' is undefined

src/audio/wma10_dec/src/Makefile.am:19:   The usual way to define `LIBTOOL' is to add `AC_PROG_LIBTOOL'

src/audio/wma10_dec/src/Makefile.am:19:   to `configure.ac' and run `aclocal' and `autoconf' again.

src/audio/wma10_dec/src/Makefile.am:19:   If `AC_PROG_LIBTOOL' is in `configure.ac', make sure

src/audio/wma10_dec/src/Makefile.am:19:   its definition is in aclocal's search path.

src/audio/wma8_enc/src/Makefile.am:5: Libtool library used but `LIBTOOL' is undefined

src/audio/wma8_enc/src/Makefile.am:5:   The usual way to define `LIBTOOL' is to add `AC_PROG_LIBTOOL'

src/audio/wma8_enc/src/Makefile.am:5:   to `configure.ac' and run `aclocal' and `autoconf' again.

src/audio/wma8_enc/src/Makefile.am:5:   If `AC_PROG_LIBTOOL' is in `configure.ac', make sure

src/audio/wma8_enc/src/Makefile.am:5:   its definition is in aclocal's search path.

src/misc/i_sink/src/Makefile.am:6: Libtool library used but `LIBTOOL' is undefined

src/misc/i_sink/src/Makefile.am:6:   The usual way to define `LIBTOOL' is to add `AC_PROG_LIBTOOL'

src/misc/i_sink/src/Makefile.am:6:   to `configure.ac' and run `aclocal' and `autoconf' again.

src/misc/i_sink/src/Makefile.am:6:   If `AC_PROG_LIBTOOL' is in `configure.ac', make sure

src/misc/i_sink/src/Makefile.am:6:   its definition is in aclocal's search path.

src/misc/v4l_sink/src/Makefile.am:1: Libtool library used but `LIBTOOL' is undefined

src/misc/v4l_sink/src/Makefile.am:1:   The usual way to define `LIBTOOL' is to add `AC_PROG_LIBTOOL'

src/misc/v4l_sink/src/Makefile.am:1:   to `configure.ac' and run `aclocal' and `autoconf' again.

src/misc/v4l_sink/src/Makefile.am:1:   If `AC_PROG_LIBTOOL' is in `configure.ac', make sure

src/misc/v4l_sink/src/Makefile.am:1:   its definition is in aclocal's search path.

src/misc/v4l_source/src/Makefile.am:7: Libtool library used but `LIBTOOL' is undefined

src/misc/v4l_source/src/Makefile.am:7:   The usual way to define `LIBTOOL' is to add `AC_PROG_LIBTOOL'

src/misc/v4l_source/src/Makefile.am:7:   to `configure.ac' and run `aclocal' and `autoconf' again.

src/misc/v4l_source/src/Makefile.am:7:   If `AC_PROG_LIBTOOL' is in `configure.ac', make sure

src/misc/v4l_source/src/Makefile.am:7:   its definition is in aclocal's search path.

src/parser/aiur/src/Makefile.am:2: Libtool library used but `LIBTOOL' is undefined

src/parser/aiur/src/Makefile.am:2:   The usual way to define `LIBTOOL' is to add `AC_PROG_LIBTOOL'

src/parser/aiur/src/Makefile.am:2:   to `configure.ac' and run `aclocal' and `autoconf' again.

src/parser/aiur/src/Makefile.am:2:   If `AC_PROG_LIBTOOL' is in `configure.ac', make sure

src/parser/aiur/src/Makefile.am:2:   its definition is in aclocal's search path.

src/video/deinterlace/src/Makefile.am:1: Libtool library used but `LIBTOOL' is undefined

src/video/deinterlace/src/Makefile.am:1:   The usual way to define `LIBTOOL' is to add `AC_PROG_LIBTOOL'

src/video/deinterlace/src/Makefile.am:1:   to `configure.ac' and run `aclocal' and `autoconf' again.

src/video/deinterlace/src/Makefile.am:1:   If `AC_PROG_LIBTOOL' is in `configure.ac', make sure

src/video/deinterlace/src/Makefile.am:1:   its definition is in aclocal's search path.

src/video/h264_dec/src/Makefile.am:21: Libtool library used but `LIBTOOL' is undefined

src/video/h264_dec/src/Makefile.am:21:   The usual way to define `LIBTOOL' is to add `AC_PROG_LIBTOOL'

src/video/h264_dec/src/Makefile.am:21:   to `configure.ac' and run `aclocal' and `autoconf' again.

src/video/h264_dec/src/Makefile.am:21:   If `AC_PROG_LIBTOOL' is in `configure.ac', make sure

src/video/h264_dec/src/Makefile.am:21:   its definition is in aclocal's search path.

src/video/ipu_csc/src/Makefile.am:6: Libtool library used but `LIBTOOL' is undefined

src/video/ipu_csc/src/Makefile.am:6:   The usual way to define `LIBTOOL' is to add `AC_PROG_LIBTOOL'

src/video/ipu_csc/src/Makefile.am:6:   to `configure.ac' and run `aclocal' and `autoconf' again.

src/video/ipu_csc/src/Makefile.am:6:   If `AC_PROG_LIBTOOL' is in `configure.ac', make sure

src/video/ipu_csc/src/Makefile.am:6:   its definition is in aclocal's search path.

src/video/mpeg2_dec/src/Makefile.am:2: Libtool library used but `LIBTOOL' is undefined

src/video/mpeg2_dec/src/Makefile.am:2:   The usual way to define `LIBTOOL' is to add `AC_PROG_LIBTOOL'

src/video/mpeg2_dec/src/Makefile.am:2:   to `configure.ac' and run `aclocal' and `autoconf' again.

src/video/mpeg2_dec/src/Makefile.am:2:   If `AC_PROG_LIBTOOL' is in `configure.ac', make sure

src/video/mpeg2_dec/src/Makefile.am:2:   its definition is in aclocal's search path.

src/video/mpeg4asp_dec/src/Makefile.am:21: Libtool library used but `LIBTOOL' is undefined

src/video/mpeg4asp_dec/src/Makefile.am:21:   The usual way to define `LIBTOOL' is to add `AC_PROG_LIBTOOL'

src/video/mpeg4asp_dec/src/Makefile.am:21:   to `configure.ac' and run `aclocal' and `autoconf' again.

src/video/mpeg4asp_dec/src/Makefile.am:21:   If `AC_PROG_LIBTOOL' is in `configure.ac', make sure

src/video/mpeg4asp_dec/src/Makefile.am:21:   its definition is in aclocal's search path.

src/video/vpu/src/Makefile.am:2: Libtool library used but `LIBTOOL' is undefined

src/video/vpu/src/Makefile.am:2:   The usual way to define `LIBTOOL' is to add `AC_PROG_LIBTOOL'

src/video/vpu/src/Makefile.am:2:   to `configure.ac' and run `aclocal' and `autoconf' again.

src/video/vpu/src/Makefile.am:2:   If `AC_PROG_LIBTOOL' is in `configure.ac', make sure

src/video/vpu/src/Makefile.am:2:   its definition is in aclocal's search path.

src/video/vpu_dec.full/src/Makefile.am:21: Libtool library used but `LIBTOOL' is undefined

src/video/vpu_dec.full/src/Makefile.am:21:   The usual way to define `LIBTOOL' is to add `AC_PROG_LIBTOOL'

src/video/vpu_dec.full/src/Makefile.am:21:   to `configure.ac' and run `aclocal' and `autoconf' again.

src/video/vpu_dec.full/src/Makefile.am:21:   If `AC_PROG_LIBTOOL' is in `configure.ac', make sure

src/video/vpu_dec.full/src/Makefile.am:21:   its definition is in aclocal's search path.

src/video/vpu_enc/src/Makefile.am:4: Libtool library used but `LIBTOOL' is undefined

src/video/vpu_enc/src/Makefile.am:4:   The usual way to define `LIBTOOL' is to add `AC_PROG_LIBTOOL'

src/video/vpu_enc/src/Makefile.am:4:   to `configure.ac' and run `aclocal' and `autoconf' again.

src/video/vpu_enc/src/Makefile.am:4:   If `AC_PROG_LIBTOOL' is in `configure.ac', make sure

src/video/vpu_enc/src/Makefile.am:4:   its definition is in aclocal's search path.

src/video/wmv9mp_dec/src/Makefile.am:2: Libtool library used but `LIBTOOL' is undefined

src/video/wmv9mp_dec/src/Makefile.am:2:   The usual way to define `LIBTOOL' is to add `AC_PROG_LIBTOOL'

src/video/wmv9mp_dec/src/Makefile.am:2:   to `configure.ac' and run `aclocal' and `autoconf' again.

src/video/wmv9mp_dec/src/Makefile.am:2:   If `AC_PROG_LIBTOOL' is in `configure.ac', make sure

src/video/wmv9mp_dec/src/Makefile.am:2:   its definition is in aclocal's search path.

src/video/wmv_dec/src/Makefile.am:2: Libtool library used but `LIBTOOL' is undefined

src/video/wmv_dec/src/Makefile.am:2:   The usual way to define `LIBTOOL' is to add `AC_PROG_LIBTOOL'

src/video/wmv_dec/src/Makefile.am:2:   to `configure.ac' and run `aclocal' and `autoconf' again.

src/video/wmv_dec/src/Makefile.am:2:   If `AC_PROG_LIBTOOL' is in `configure.ac', make sure

src/video/wmv_dec/src/Makefile.am:2:   its definition is in aclocal's search path.

tools/gplay/Makefile.am:1: Libtool library used but `LIBTOOL' is undefined

tools/gplay/Makefile.am:1:   The usual way to define `LIBTOOL' is to add `AC_PROG_LIBTOOL'

tools/gplay/Makefile.am:1:   to `configure.ac' and run `aclocal' and `autoconf' again.

tools/gplay/Makefile.am:1:   If `AC_PROG_LIBTOOL' is in `configure.ac', make sure

tools/gplay/Makefile.am:1:   its definition is in aclocal's search path.

Makefile.am:972: `%'-style pattern rules are a GNU make extension

+ exit 1

error: Bad exit status from /home/jci/ltib_test/ltib/tmp/rpm-tmp.25237 (%build)

RPM build errors:

    Bad exit status from /home/jci/ltib_test/ltib/tmp/rpm-tmp.25237 (%build)

Build time for gst-fsl-plugins: 12 seconds

Failed building gst-fsl-plugins

f_buildrpms() returned an error, exiting

traceback:

main:572

Started: Mon Nov 25 10:50:06 2013

Ended:   Mon Nov 25 10:50:55 2013

Elapsed: 49 seconds

These packages failed to build:

gst-fsl-plugins

Build Failed

Exiting on error or interrupt

1 解答
1,388 次查看
ketandeshpande
Contributor I

Hi,

Solved the issue. libtool was missing from my system. Had to install it and got everything working again

$ sudo apt-get install libtool

did the trick.

Thanks & Regards,

- Ketan

在原帖中查看解决方案

2 回复数
1,389 次查看
ketandeshpande
Contributor I

Hi,

Solved the issue. libtool was missing from my system. Had to install it and got everything working again

$ sudo apt-get install libtool

did the trick.

Thanks & Regards,

- Ketan

1,388 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Ketan,

I see you have solved your problem, would you please click Corect Answer/Helpful Answer. We would assume your issue/question got answered if no response from you in 3 days and close the DI. Thanks a lot.

Any other questions will be welcome~~

Best Regards

Dan

0 项奖励
回复