graphics version

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

graphics version

1,775件の閲覧回数
erikraynolds
Contributor IV

Documentation says:

The kernel module version of graphics used on the system can be found by running the following command on the board:
dmesg | grep Galcore

I got response:

root@imx6qpsabreauto:~# dmesg | grep Galcore
[ 0.836271] Galcore version 5.0.11.41671

The user-side GPU drivers version of graphics can be displayed using the following command on the board:
grep VERSION /usr/lib/libGAL*

root@imx6qpsabreauto:~# grep VERSION /usr/lib/libGAL*
Binary file /usr/lib/libGAL.so matches

I'm not getting version number: What's the GPU drivers version?

タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,646件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Erick:

This may help:

https://community.nxp.com/thread/308582 

regards

0 件の賞賛
返信

1,646件の閲覧回数
erikraynolds
Contributor IV

Nope your link did not help. 

0 件の賞賛
返信