gputop: libgpuperfcnt can't be found

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

gputop: libgpuperfcnt can't be found

2,361件の閲覧回数
vmbtech
Contributor I

Hi there, trying to build gputop and it seems I need libgpuperfcnt

https://source.codeaurora.org/external/imx/imx-gputop/

I see in meta-freescale/SCR/SCR-5.15.5-1.0.0.txt the following references to it, but not sure how I can get a link to download it or if it has any source files which I'm sure I will need

Package:                     libgpuperfcnt-6.4.3.p4.0-aarch64-wayland.bin
Version:                     6.4.3.p4.0
Outgoing License:            LA_OPT_NXP_Software_License v34 February 2022 - Additional distribution license granted - Section 2.3 applies
License File:                COPYING
Package Category:            Graphics
Type of Content:             binary
Description and comments:    Library to retrieve i.MX GPU performance data
Release Location:            Mirror
Origin:                      NXP (proprietary)

--------------------------------------------

Package:                     libgpuperfcnt-6.4.3.p4.0-arm-fb.bin
Version:                     6.4.3.p4.0
Outgoing License:            LA_OPT_NXP_Software_License v34 February 2022 - Additional distribution license granted - Section 2.3 applies
License File:                COPYING
Package Category:            Graphics
Type of Content:             binary
Description and comments:    Library to retrieve i.MX GPU performance data
Release Location:            Mirror
Origin:                      NXP (proprietary)

--------------------------------------------

Package:                     libgpuperfcnt-6.4.3.p4.0-arm-wayland.bin
Version:                     6.4.3.p4.0
Outgoing License:            LA_OPT_NXP_Software_License v34 February 2022 - Additional distribution license granted - Section 2.3 applies
License File:                COPYING
Package Category:            Graphics
Type of Content:             binary
Description and comments:    Library to retrieve i.MX GPU performance data
Release Location:            Mirror
Origin:                      NXP (proprietary)

0 件の賞賛
返信
2 返答(返信)

2,344件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

gputop and libgpuperfcnt builds for linux BSP seem broken in 5.15 indeed. You have to enter a case (make sure you have nda) to attached to the thread patches for the makefiles so you can build. 

Before running the command, you would need to enable vProfiler option as described in  "12.6.3.1 Enable vProfiler option in kernel" from "i.MX Graphics User's Guide" in order to get proper occupancy values.

Regards

0 件の賞賛
返信

2,161件の閲覧回数
ChristianPrather
Contributor II

Hello, has this been resolved? When attempting to build libgpuperfcnt bb file I get the following fetch error. 


libgpuperfcnt-6.4.3.p4.6-r0 do_fetch: Failed to fetch URL https://www.nxp.com/lgfiles/NMG/MAD/YOCTO//libgpuperfcnt-6.4.3.p4.6-aarch64-fb.bin;fsl-eula=true;nam..., attempting MIRRORS if available

Seems like there is a missing bin in the lgfiles dir or the link is incorrect. Any assistance would be greatly appreciated.

Related Issue:

https://community.nxp.com/t5/i-MX-Processors/libgpuperfcnt-6-4-3-p1-4-can-t-be-fetched-in-Yocto-Zeus...