gpu-viv-bin-mx6q buildroot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

gpu-viv-bin-mx6q buildroot

Jump to solution
5,839 Views
richc128
Contributor III

Is there a way to integrate the gpu-viv-bin-mx6q package in buildroot?

I can only extract these binaries over the rootfilesystem. But, they seem to be built with a compilar that I can't seem to find. I did try the one included with ltib with no luck.

Are there sources for these binaries?

http://repository.timesys.com/buildsources/g/gpu-viv-bin-mx6q/

Labels (2)
0 Kudos
Reply
1 Solution
3,467 Views
andre_silva
NXP Employee
NXP Employee

Hi Richard,

the integration only can be done using the package you got in this link, unfortunately the source code is not provided.

To have access to the source codes you need to contact freescale via customer support service and ask for the source. In this case, you will need to do some agreements and accept the terms and conditions to have access to it.

regards,

Andre

View solution in original post

0 Kudos
Reply
5 Replies
3,468 Views
andre_silva
NXP Employee
NXP Employee

Hi Richard,

the integration only can be done using the package you got in this link, unfortunately the source code is not provided.

To have access to the source codes you need to contact freescale via customer support service and ask for the source. In this case, you will need to do some agreements and accept the terms and conditions to have access to it.

regards,

Andre

0 Kudos
Reply
3,467 Views
richc128
Contributor III

Don’t suppose you have contact info?

0 Kudos
Reply
3,467 Views
andre_silva
NXP Employee
NXP Employee

Yes it was, but it has to be done via Customer support.

0 Kudos
Reply
3,467 Views
richc128
Contributor III

Thanks. I’ve submitted a ticket.

0 Kudos
Reply
3,467 Views
andre_silva
NXP Employee
NXP Employee

thank you.

0 Kudos
Reply