gpu-viv-bin-mx6q buildroot

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

gpu-viv-bin-mx6q buildroot

跳至解决方案
5,821 次查看
richc128
Contributor III

Is there a way to integrate the gpu-viv-bin-mx6q package in buildroot?

I can only extract these binaries over the rootfilesystem. But, they seem to be built with a compilar that I can't seem to find. I did try the one included with ltib with no luck.

Are there sources for these binaries?

http://repository.timesys.com/buildsources/g/gpu-viv-bin-mx6q/

标签 (2)
0 项奖励
回复
1 解答
3,449 次查看
andre_silva
NXP Employee
NXP Employee

Hi Richard,

the integration only can be done using the package you got in this link, unfortunately the source code is not provided.

To have access to the source codes you need to contact freescale via customer support service and ask for the source. In this case, you will need to do some agreements and accept the terms and conditions to have access to it.

regards,

Andre

在原帖中查看解决方案

0 项奖励
回复
5 回复数
3,450 次查看
andre_silva
NXP Employee
NXP Employee

Hi Richard,

the integration only can be done using the package you got in this link, unfortunately the source code is not provided.

To have access to the source codes you need to contact freescale via customer support service and ask for the source. In this case, you will need to do some agreements and accept the terms and conditions to have access to it.

regards,

Andre

0 项奖励
回复
3,449 次查看
richc128
Contributor III

Don’t suppose you have contact info?

0 项奖励
回复
3,449 次查看
andre_silva
NXP Employee
NXP Employee

Yes it was, but it has to be done via Customer support.

0 项奖励
回复
3,449 次查看
richc128
Contributor III

Thanks. I’ve submitted a ticket.

0 项奖励
回复
3,449 次查看
andre_silva
NXP Employee
NXP Employee

thank you.

0 项奖励
回复