gpu & vpu probe issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

gpu & vpu probe issue

Jump to solution
4,988 Views
zohanlin
Contributor IV

Dear guys,

 

I have one OS yocto 2.4 rock (kernel 4.9.88) which runs in imx6q, the gpu and vpu work well.

So I try another OS yocto 3.1 Zeus(kernel 5.4.47)which runs in imx6q, the gpu and vpu don't work.

Log as below

 

[    3.850835] galcore 130000.gpu: ignoring dependency for device, assuming no driver
[    3.858990] mxc_vpu 2040000.vpu_fsl: ignoring dependency for device, assuming no driver

 

 

 

Could somebody help me?

 

 

 

0 Kudos
Reply
1 Solution
4,929 Views
zohanlin
Contributor IV

Hi igor,

I found the reason that is my custom board remove the pmic.

So I comment some dts item as below

/*
&reg_arm {
       vin-supply = <&sw1a_reg>;
};

&reg_pu {
       vin-supply = <&sw1c_reg>;
};

&reg_soc {
       vin-supply = <&sw1c_reg>;
};
*/

 

Now the GPU & VPU can work well.

View solution in original post

5 Replies
4,981 Views
igorpadykov
NXP Employee
NXP Employee

Hi zohanlin

 

one can try to test vpu,gpu on nxp sabresd reference board with Demo Image

i.MX 6QuadPlus, i.MX 6Quad, i.MX 6DualLite, i.MX 6SoloX Boards​

https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat...

 

Best regards
igor

0 Kudos
Reply
4,930 Views
zohanlin
Contributor IV

Hi igor,

I found the reason that is my custom board remove the pmic.

So I comment some dts item as below

/*
&reg_arm {
       vin-supply = <&sw1a_reg>;
};

&reg_pu {
       vin-supply = <&sw1c_reg>;
};

&reg_soc {
       vin-supply = <&sw1c_reg>;
};
*/

 

Now the GPU & VPU can work well.

4,954 Views
zohanlin
Contributor IV

I found a post about the issue.

https://community.nxp.com/t5/i-MX-Processors/Problem-with-galcore-GPU-module-on-imx6-Solo/td-p/10560... 

 

Bio_TICFSL said : Sorry and yes the issue is on DTBs.

Is it really?

 

0 Kudos
Reply
4,962 Views
zohanlin
Contributor IV

Hi igor,

My board is not EVK, so I could not test the demo image.

I downloaded linux-imx 5.4.70, and the version has the same problem.

Could you have other suggestions?

 

0 Kudos
Reply
4,982 Views
zohanlin
Contributor IV

I tried to modify dts and set #power-domain-cells by <1>

--------------------------------------------------------------------------

pd_pu: power-domain@1 {
reg = <1>;
#power-domain-cells = <1>;
power-supply = <&reg_pu>;
clocks = <&clks IMX6QDL_CLK_GPU3D_CORE>,
<&clks IMX6QDL_CLK_GPU3D_SHADER>,
<&clks IMX6QDL_CLK_GPU2D_CORE>,
<&clks IMX6QDL_CLK_GPU2D_AXI>,
<&clks IMX6QDL_CLK_OPENVG_AXI>,
<&clks IMX6QDL_CLK_VPU_AXI>;
};

 

Now the log is

root@imx6qsabresd:~# dmesg | grep -i "gpu"
[ 3.628942] OF: /soc/gpu@00130000: #power-domain-cells = 1 found -1
[ 4.328302] galcore: probe of 130000.gpu failed with error -22


root@imx6qsabresd:~# dmesg | grep -i "gal"
[ 3.291714] egalax_ts 1-0004: Failed to switch to I2C interface
[ 3.298098] egalax_ts 2-0004: Failed to switch to I2C interface
[ 3.636502] Galcore version 6.4.3.p0.286725
[ 4.291168] [galcore]: Feature database is not found,chipModel=0x0, chipRevision=0x0, productID=0x0, ecoID=0x0, customerID=0x0
[ 4.328302] galcore: probe of 130000.gpu failed with error -22

root@imx6qsabresd:~# dmesg | grep -i "vpu"
[ 4.334554] OF: /soc/aips-bus@2000000/vpu_fsl@2040000: #power-domain-cells = 1 found -1
[ 4.343296] mxc_vpu 2040000.vpu_fsl: VPU initialized

0 Kudos
Reply