gpio status reading from mfgtool script

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

gpio status reading from mfgtool script

1,298 Views
shabeerbadarudh
Contributor IV

Hi All,

We need to write a generic mfgtool scrtipt for the different versions of a similler hardware. These hardware provides some gpios for indicating the hardware revision. Our aim is to flash  different binaries by reading these gpio states. So is it possible to read the gpio status from the mfgtool (ucl script)?.  

I have gone through the 'Manufacturing Tool V2 (MFGTool2) Update Command List (UCL) User Guide.doc', which explains some 'Firmware Specific Commands' like 'read'. Is it possible to read gpio state using this types of commands or any other mechanisms available for reading the gpio states.

Thanks,

Shabeer

0 Kudos
Reply
1 Reply

1,139 Views
alejandrolozan1
NXP Employee
NXP Employee

Hi,

It seems that you may need to get the mfgtool source code and recompile it. According to this

MFG tool. Is it possible to read from flash

Apps\MfgTool.exe\OpUtpUpdate.cpp may be helpful.

Best Regards,

Alejandro