google chrome on imx6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

google chrome on imx6

3,088 次查看
sameerarvikar
Contributor III

Hi ,

I want to install google chrome on imx6 on linux ,

Which yocto version supports it .

I know chromium browser can be install ,but is it possible to install chrome

thanks & regards

标记 (3)
0 项奖励
回复
1 回复

2,139 次查看
CarlosCasillas
NXP Employee
NXP Employee

Hi,

From NXP Yocto BSP side, just the Chromium recipe is available. Another option could be using a different Linux BSP for i.MX6 with Chrome support, like Ubuntu and try on it:

You could take a look at the following link:

https://community.nxp.com/docs/DOC-330147

Hope this will be useful for you.

Best regards!

/Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复