google chrome on imx6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

google chrome on imx6

2,540件の閲覧回数
sameerarvikar
Contributor III

Hi ,

I want to install google chrome on imx6 on linux ,

Which yocto version supports it .

I know chromium browser can be install ,but is it possible to install chrome

thanks & regards

タグ(3)
0 件の賞賛
返信
1 返信

1,591件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi,

From NXP Yocto BSP side, just the Chromium recipe is available. Another option could be using a different Linux BSP for i.MX6 with Chrome support, like Ubuntu and try on it:

You could take a look at the following link:

https://community.nxp.com/docs/DOC-330147

Hope this will be useful for you.

Best regards!

/Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信