git merge between android and linux source code for toradex apalis imx6 processor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

git merge between android and linux source code for toradex apalis imx6 processor

2,181 Views
vinothkumars
Senior Contributor IV

Dear NXP,

I want to port the android 8 (i.MX Software | NXP ) in one of the Toradex board.

But, Toradex supports Linux only (Build U-Boot and Linux Kernel from Source Code ). So, i plan to merge the source code of android 8 with Linux. But, i do not know how to merge these two sources. And also in linux i got u-boot as well as linux for toradex.

but, in android i got complete source. So, how will merge the two different sources ?

Regards,

VinothS

Regards,
Vinothkumar Sekar
Labels (4)
0 Kudos
Reply
2 Replies

2,106 Views
igorpadykov
NXP Employee
NXP Employee

Hi VinothS

one can look at below linux (Porting Guide) and android documentation :

i.MX Software | NXP 

Android Porting - eLinux.org 

Design an Android Device  |  Android Open Source Project 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,106 Views
vinothkumars
Senior Contributor IV

Thank you Igore, I closed this thread now.

Regards,

VinothS

Regards,
Vinothkumar Sekar
0 Kudos
Reply