git://git.freescale.com/imx/linux-imx.git is down again

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

git://git.freescale.com/imx/linux-imx.git is down again

10,186 次查看
lakehu
Contributor II

Hi 

I try several places to clone this week. All fail.

The git server web access is OK, however, git clone can't be successful.

$ git clone git://git.freescale.com/imx/imx-firmware.git
Cloning into 'imx-firmware'...
fatal: unable to connect to git.freescale.com:
git.freescale.com[0: 192.88.156.202]: errno=Connection timed out

What happened??

标签 (3)
标记 (1)
0 项奖励
回复
4 回复数

4,546 次查看
tmatsuzawa
Contributor I

Hello, I am also seeing this and seeking a solution.

1) errors

I am also seeing folowing errors since yesterday (as far as I am aware)

>fatal: unable to connect to git.freescale.com:
git.freescale.com[0: 192.88.156.202]: errno=Connection timed out


>fatal: unable to connect to git.freescale.com:
git.freescale.com[0: 192.88.156.202]: errno=Connection timed out

For my command like below, which used to work.

>repo init -u git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-4.1-krogoth -m imx-4.1.15-2.0.0-agl-demo.xml

2) workaround

This maybe server side fault, but since I can see these repository on cgit share, I tried following

(in ~/.gitconfig)

>[url "https://git.freescale.com/git/cgit.cgi/imx"]
> insteadOf = git://git.freescale.com/imx

Initially this seemed to work, but I get the following erros.

>fatal: https://git.freescale.com/git/cgit.cgi/imx/meta-fsl-bsp-release/info/refs not valid: is this a git repository?
>fatal: https://git.freescale.com/git/cgit.cgi/imx/meta-nxp-agl/info/refs not valid: is this a git repository?

I guess URL constructed by repo command internally is not valid so I am seeing this error.

But I am unable to find a right workaround.

In case accssing via https is safer/more stable, I would like to use that, but in such case I want to know what is the right customization in .gitconfig.

0 项奖励
回复

4,546 次查看
Carlos_Musich
NXP Employee
NXP Employee

Hi, we are working internally to get this resolved.   The GIT managers are aware of the issue and we are working to find the root cause and solution.  In the meantime, you can navigate to the GIT website in web browser and download packages from there.   We hope to have it resolved soon.


Best regards,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

4,546 次查看
canfengwen
Contributor II

Hi Carlos,

Seems the git server is still not stable? i'm also failed to clone the code due the connection refused issue. 

0 项奖励
回复

4,546 次查看
lakehu
Contributor II

Can anyone help? 

Thanks

0 项奖励
回复