git.freescale.com down?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

git.freescale.com down?

12,127件の閲覧回数
daveschiopucie
Contributor I

Trying to sync to git.freescale.com, getting "Unable to connect go git.freescale.com".

Did something change?

DS

18 返答(返信)

10,077件の閲覧回数
dhananjay_chauh
Contributor I

I am facing this issue now.

USING REPO INIT:

repo init -u git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-4.1-krogoth

 

manifests:
fatal: unable to connect to git.freescale.com:
git.freescale.com[0: 192.88.156.202]: errno=Connection refused

Is there an issue with the server? I am facing this issue from 29/02/2020.

0 件の賞賛
返信

10,077件の閲覧回数
fsiegel
Contributor I

I'm having troubles cloning linux-imx specifically imx_4.1.15_2.0.0_ga.

Running bitbake I get:

fatal: The remote end hung up unexpectedly
fatal: early EOF
fatal: index-pack failed

ERROR: linux-imx-4.1.15-r0 do_fetch: Function failed: Fetcher failure for URL: 'git://git.freescale.com/imx/linux-imx.git;protocol=git;branch=imx_4.1.15_2.0.0_ga'. Unable to fetch URL from any source.

after some time or:

fatal: Could not read from remote repository.

Please make sure you have the correct access rights
and the repository exists.

ERROR: linux-imx-4.1.15-r0 do_fetch: Function failed: Fetcher failure for URL: 'git://git.freescale.com/imx/linux-imx.git;protocol=git;branch=imx_4.1.15_2.0.0_ga'. Unable to fetch URL from any source.

when it fails immediately.

Cloning manually also fails with either early end of file or could not read.

Didn't work yesterday either, but used to last week.

U-Boot do_fetch() completed on the second attempt.

Cloning from Github works fine so I guess the freescale repository is having hickups again.

(A Mirror would be great for this case)

10,078件の閲覧回数
Danube
Contributor IV

Hi ,

I  try more than 5 times and download finish.

(Command  : bitbake -c fetchall linux-imx)

0 件の賞賛
返信

10,078件の閲覧回数
keestrommel
Contributor IV

Today having the same problem.

Because this is a re-occurring issue a mirror would very helpful.

0 件の賞賛
返信

10,077件の閲覧回数
tomfoy
Contributor II

I've advised our local NXP rep, but no real response yet, like ETA etc...

10,077件の閲覧回数
chetkaufman
NXP Employee
NXP Employee

Hi, we are working internally to get this resolved.   The GIT managers are aware of the issue and we are working to find the root cause and solution.  In the meantime, you can navigate to the GIT website and download packages from there.   We hope to have it resolved soon.  

0 件の賞賛
返信

10,077件の閲覧回数
chetkaufman
NXP Employee
NXP Employee

Hi all, I was told that our GIT repository is fixed now and cloning should work.   Please post on this thread if you are still seeing issues so I can alert the team that more work is needed.  

10,077件の閲覧回数
cyrilstrejc
Contributor III

I think the following git clone used to work, but not anymore...

$ git clone git://git.freescale.com/ppc/sdk/usdpaa/usdpaa-apps.git

Cloning into 'usdpaa-apps'...
fatal: unable to connect to git.freescale.com:
git.freescale.com[0: 192.88.156.202]: errno=Connection refused
0 件の賞賛
返信

10,077件の閲覧回数
jonathanwebster
Contributor II

This works for me now:-

$ repo init -u git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-4.1-krogoth

10,077件の閲覧回数
cyrilstrejc
Contributor III

Yes, even that my git clone works now. The Freescale's git repo seems to be OK completely.

10,078件の閲覧回数
rowangifford
Contributor II

Any replys from NXP? Are they aware of the issue?

0 件の賞賛
返信

10,077件の閲覧回数
jedrumh75
Contributor I

No replies that I noticed. I tried sharing this post to hopefully gain exposure. You could also try doing the same. 

0 件の賞賛
返信

10,078件の閲覧回数
jonathanwebster
Contributor II

I've not seen any responses from NXP.

How do we prompt them?

0 件の賞賛
返信

10,078件の閲覧回数
alexanderchubuc
Contributor I

I get the same error

0 件の賞賛
返信

10,078件の閲覧回数
jedrumh75
Contributor I

I'm also experiencing the same issue. Have been since May 6, 2017

0 件の賞賛
返信

10,078件の閲覧回数
rowangifford
Contributor II

Also getting either connection refused or timeout

0 件の賞賛
返信

10,077件の閲覧回数
tomfoy
Contributor II

I am also experiencing this problem today.

0 件の賞賛
返信

10,078件の閲覧回数
jonathanwebster
Contributor II

That could be what I'm seeing as well!

https://community.nxp.com/thread/450783