gicv3 interrupt init, interrupt trigger, interrupt handler at uboot command ( EL2 mode )

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

gicv3 interrupt init, interrupt trigger, interrupt handler at uboot command ( EL2 mode )

2,369 Views
dongjoo99kim
Contributor I

Dear all.

 

I have developed imx8mq including cortex a53, gicv3 controller.

 

As i know, uboot can't support gicv3 interrupt init, interrupt trigger, interrupt handler by the uboot exception vector table.

But, I want to bring up gicv3 interrupt init, interrupt trigger, interrupt handler by the uboot exception vector table not routing to El1 or El3.

And, our uboot run at el2 mode.

 

My scenario is to bring up a gicv3 interrupt init, interrupt trigger at uboot command.

After trigger interrupt at uboot command, I want to get a interrupt handler by the uboot execption vector table not routing to EL1 or El3.

 

Is there any method to solve this problem?

Please, help me.

 

Thanks.

 

0 Kudos
Reply
3 Replies

2,354 Views
Hariharan1
Contributor III

HI, How do you flash uboot binary into sd card. I am also flashed but it shows invalid partition 1. what are the things need to prepare sd card before flashing. can you share your thoughts?

BuildInfo:
- ATF 70fa7bc
- U-Boot 2019.04-04771-g4d377539a1

Run CMD11 1.8V switch
switch to partitions #0, OK
mmc1 is current device
flash target is MMC:1
Run CMD11 1.8V switch
Net:
Warning: ethernet@30be0000 using MAC address from ROM
eth0: ethernet@30be0000
Fastboot: Normal
Normal Boot
Hit any key to stop autoboot: 0
Run CMD11 1.8V switch
switch to partitions #0, OK
mmc1 is current device
Run CMD11 1.8V switch
** Invalid partition 1 **
** Invalid partition 1 **
Booting from net ...

Thanks,

0 Kudos
Reply

2,332 Views
dongjoo99kim
Contributor I

Dear Hariharan1 

 

I just copy the uboot image using usb sdcard reader from host PC.

Sorry. But, I can't answer the method to you what  you request. 

 

Could you share to me the method  how to enable gicv3 interrupt init, interrupt trigger, interrupt handler at uboot cvommand ( EL2 mode) ?

 

Thanks. 

0 Kudos
Reply

2,317 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

g

0 Kudos
Reply