Hi All
I am booting i.MX6q board and getting below error:-
starting kernel...
data abort
MAYBE you should read doc/README.arm-unaligned-accesses
I used the below steps to burn SD card:-
1. copy the u-boot image by using
sudo dd if=u-boot-imx6qsabresd_sd.imx of=/dev/sdb bs=512 seek=2 conv=fsync
2. copy the kernel image by using
sudo dd if=uImage_imx_v7_defconfig of=/dev/sdb bs=512 seek=2048 conv=fsync
3. copy DTB file by using
sudo dd if=uImage-imx6q-sabresd.dtb of=/dev/sdb bs=512 seek=20480 conv=fsync
4. copy the file system using
sudo mkfs.ext3 /dev/sdb1
sudo mount /dev/sdb1 /mount
sudo mount -o loop -t ext3 fsl-image-fb-imx6qdlsolo.ext3 /home/user/rootfs
cd /home/user/rootfs
sudo cp -a * /mount
sudo umount /mount
sudo umount /jome/user/rootfs
Then I used following steps to boot iMX6q board suing U-Boot:-
1. setenv loadaddr 0x12000000
2. setenv fdt_addr 0x18000000
3. setenv fdt_high 0xffffffff
4. setenv bootargs_base 'setenv bootargs console-ttymxc0,115200'
5. setenv bootargs_mmc 'setenv bootargs ${bootargs} root=/dev/mmcblk0p2 rootwait rw video=mxcfb1:dev=ldb,LDB-XGA, if=RGB666 video=mxcfb0:dev=hdmi,1920x1080M@60, if=RGB24'
6. setenv bootcmd_mmc 'run bootargs_base bootargs_mmc;mmc dev 1;mmc read ${loadaddr} 0x800 0x3000;mmc read ${ftd_addr} 0x5000 0x9C;bootm ${loadaddr} - ${ftd_addr}'
7. setenv bootcmd 'run bootcmd_mmc'
8. saveenv
9. run bootcmd
Thanks
Virendra singh
 
					
				
		
 Yuri
		
			Yuri
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Have You tried to test memory for assurance ?
"i.Mx6DQSDL DDR3 Script Aid"
https://community.freescale.com/docs/DOC-94917 
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------