fw_printenv(fw_setenv ) read from (write to ) which partition on sdcard for maaxboard(imx8mq_dev)?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

fw_printenv(fw_setenv ) read from (write to ) which partition on sdcard for maaxboard(imx8mq_dev)?

1,928 次查看
gonewithwind-peter
Senior Contributor I

Hi all 

I want to solve my Qz here 

running uboot 's saveenv damage boot partition and can not boot again on maaxboard

https://community.nxp.com/t5/i-MX-Processors/running-uboot-s-saveenv-damage-boot-partition-and-can-n...

so I have to know that  fw_printenv(fw_setenv ) read from (write to ) which partition on sdcard?

I following the guide here: https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Linux-fw-printenv-fw-setenv-to-access-U-...

I am play rauc , so I add one more addition rootfs. there are following partitions (using lsblck or gparted to show) in my bootable sdcard:

mmcblk0p1    (boot partition, kernel image, dtb uEnv.txt in it)   (notes: uboot image is msdos. can not show with lsblk)

mmcblk0p2 (rootfs_A)   normally mount at  /  after bootup

mmcblk0p3 (rootfs_B)    I want to switch it using rauc.

condition 1:

I tried first with   file: /etc/fw_env.conf  

/dev/mmcblk0  0x400000 0x1000

 

I can successfully run  fw_printenv and fw_setenv  ,

my Qz  1: at  /dev/mmcblk0  , fw_printenv(fw_setenv ) read from (write to ) which partition?    mmcblk0p1 ?  mmcblk0p2?

 

condition 2:

I tried secondly  with   file: /etc/fw_env.conf  

/dev/mmcblk0p1  0x400000 0x1000

 I can successfully run  fw_printenv and fw_setenv   and I can set different content environment variable with  condition 1.     and  both condition 1 and 2  can exist same time. if I change the file /etc/fw_env.conf  .I can  fw_printenv different content that I set before.

 

my Qz: so I condition 2 the environment variable is in which partition?  mmcblk0p1 ?  mmcblk0p2? ??? 

 

I was confused.

any help ?

Thank you very much.

 

 

 

 

 

 

 

0 项奖励
回复
4 回复数

1,907 次查看
jimmychan
NXP TechSupport
NXP TechSupport

Please try to dump the contents in the SD card. Check the changes are properly write to the correct offset in the storage.

0 项奖励
回复

1,890 次查看
gonewithwind-peter
Senior Contributor I
it seem I set define CONFIG_ENV_OFFSET in .h file in uboot code is not work
#define CONFIG_ENV_OFFSET 0x2904000


it still savenev at 0x400000 (that is default setting for imx) (64 * SZ_64K) in sdcard and just damage the boot partition
it seems my setting is not working and can not change the default setting. but I wrote a wrong syntax to compile the code. it displayed error and I made sure it was compiled.
Let me try again.
0 项奖励
回复

1,895 次查看
gonewithwind-peter
Senior Contributor I

Hi
@jimmychan
thank you very much for your reply.
I think that is a good idea to dump the contents in the SD card to find the ENV position. but I do not how to dump.
before I tried to write c code to read /dev/mmcblk0 ,but the code not work. and I tried dd , but I did know what the options.
do you have more details to dump the contents in the SD card?
Thank you very much.

 

I have found the dd command how to dump, thanks

https://imxdev.gitlab.io/tutorial/How_to_dump_the_SDCard_content_to_an_image_file/

0 项奖励
回复

1,892 次查看
gonewithwind-peter
Senior Contributor I

I find partial answer

 /etc/fw_env.conf 

/dev/mmcblk0  0x400000 0x1000 and the fw_printenv will damage the boot partition.

if /dev/mmcblk 0x2904000 0x1000    fw_printenv fw_setenv will work well. 

 

fw_printenv should write to absolute address  0x400000 (0x2904000) from sd card 0 sector 

I am searching saveenv in uboot command  to write where and calculate  how to set .h  file in uboot source code.

 

 

it seem I set define CONFIG_ENV_OFFSET in .h file in uboot code is not work
#define CONFIG_ENV_OFFSET 0x2904000


it still savenev at 0x400000 (that is default setting for imx) (64 * SZ_64K) in sdcard and just damage the boot partition
it seems my setting is not working and can not change the default setting. but I wrote a wrong syntax to compile the code. it displayed error and I made sure it was compiled.
Let me try again.

 

0 项奖励
回复