fsl-image-validation-imx build failed

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

fsl-image-validation-imx build failed

10,956件の閲覧回数
alexeymodyanov
Contributor II

I use latest 4.14.98_2.0.0_ga version and try to build an image for imx6qp Sabre board

I use bitbake fsl-image-validation-imx command

Host system  Ubuntu 16.04

Here is part of log:

git -c core.fsyncobjectfiles=0 checkout -B imx_18.11 64441b79b83e0790008486779054e9da891537f3 failed with exit code 128, output:
git-lfs smudge -- 'data/images/1280x720.ppm': 1: git-lfs smudge -- 'data/images/1280x720.ppm': git-lfs: not found
error: external filter git-lfs smudge -- %f failed -1
error: external filter git-lfs smudge -- %f failed
fatal: data/images/1280x720.ppm: smudge filter lfs failed

ERROR: arm-compute-library-18.11+gitAUTOINC+64441b79b8-r0 do_unpack: Function failed: base_do_unpack

if I try to execute commands just in command line all works fine.

ラベル(3)
8 返答(返信)

9,711件の閲覧回数
jay_park
Contributor II

I got a same issue and solve it by adding a symbolic link of git-lfs in build/tmp/hosttools directory.

imx-yocto-bsp/build/tmp/hosttools$ ln -sf /usr/bin/git-lfs git-lfs

Hope it helps you. 

9,958件の閲覧回数
luciomonteros
Contributor I

The same happens to me in my imx8mq. Does anyone solve this error?

0 件の賞賛
返信

10,312件の閲覧回数
khang_letruong1
Contributor I

Hello All,

I've got same error by doing following commands as in the i.MX_Yocto_Project_User's_Guide.pdf :

$ repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-sumo -m imx-4.14.98-2.0.0_ga.xml
$ repo sync

$ DISTRO=fsl-imx-wayland MACHINE=imx8mmevk source fsl-setup-release.sh -b build-wayland
$ bitbake fsl-image-validation-imx

My laptop runs Ubuntu-16.04. What should I do?

Thanks in advance,

0 件の賞賛
返信

10,312件の閲覧回数
gn02380756
Contributor II

Hi Radhika Somaiya:

I faced the same problem when building imx6qsabresd, following is my error log.

build_error.PNG

I'm sure I had installed git-lfs, but the error still occurred. Can you please solve this problem? Thanks!

10,224件の閲覧回数
rohit_k
Contributor I

Hello,

I am also getting same error  while compilation..

Please see logs.

ERROR: arm-compute-library-18.11+gitAUTOINC+64441b79b8-r0 do_unpack: Fetcher failure: Fetch command export PSEUDO_DISABLED=1; export DBUS_SESSION_BUS_ADDRESS="unix:abstract=/tmp/dbus-3BLvOBVse5"; export SSH_AUTH_SOCK="/run/user/1000/keyring/ssh"; export PATH="/home/rohit/Desktop/sumo_var_setup/var-fsl-yocto/sources/poky/scripts:/home/rohit/Desktop/sumo_var_setup/var-fsl-yocto/build_xwayland/tmp/work/aarch64-poky-linux/arm-compute-library/18.11+gitAUTOINC+64441b79b8-r0/recipe-sysroot-native/usr/bin/aarch64-poky-linux:/home/rohit/Desktop/sumo_var_setup/var-fsl-yocto/build_xwayland/tmp/work/aarch64-poky-linux/arm-compute-library/18.11+gitAUTOINC+64441b79b8-r0/recipe-sysroot/usr/bin/crossscripts:/home/rohit/Desktop/sumo_var_setup/var-fsl-yocto/build_xwayland/tmp/work/aarch64-poky-linux/arm-compute-library/18.11+gitAUTOINC+64441b79b8-r0/recipe-sysroot-native/usr/sbin:/home/rohit/Desktop/sumo_var_setup/var-fsl-yocto/build_xwayland/tmp/work/aarch64-poky-linux/arm-compute-library/18.11+gitAUTOINC+64441b79b8-r0/recipe-sysroot-native/usr/bin:/home/rohit/Desktop/sumo_var_setup/var-fsl-yocto/build_xwayland/tmp/work/aarch64-poky-linux/arm-compute-library/18.11+gitAUTOINC+64441b79b8-r0/recipe-sysroot-native/sbin:/home/rohit/Desktop/sumo_var_setup/var-fsl-yocto/build_xwayland/tmp/work/aarch64-poky-linux/arm-compute-library/18.11+gitAUTOINC+64441b79b8-r0/recipe-sysroot-native/bin:/home/rohit/Desktop/sumo_var_setup/var-fsl-yocto/sources/poky/bitbake/bin:/home/rohit/Desktop/sumo_var_setup/var-fsl-yocto/build_xwayland/tmp/hosttools"; export HOME="/home/rohit"; git -c core.fsyncobjectfiles=0 checkout -B imx_18.11 64441b79b83e0790008486779054e9da891537f3 failed with exit code 128, output:
git-lfs smudge -- 'data/images/1280x720.ppm': 1: git-lfs smudge -- 'data/images/1280x720.ppm': git-lfs: not found
error: external filter git-lfs smudge -- %f failed -1
error: external filter git-lfs smudge -- %f failed
fatal: data/images/1280x720.ppm: smudge filter lfs failed

ERROR: arm-compute-library-18.11+gitAUTOINC+64441b79b8-r0 do_unpack: Function failed: base_do_unpack
ERROR: Logfile of failure stored in: /home/rohit/Desktop/sumo_var_setup/var-fsl-yocto/build_xwayland/tmp/work/aarch64-poky-linux/arm-compute-library/18.11+gitAUTOINC+64441b79b8-r0/temp/log.do_unpack.4789
ERROR: Task (/home/rohit/Desktop/sumo_var_setup/var-fsl-yocto/sources/meta-fsl-bsp-release/imx/meta-sdk/recipes-support/arm-compute-library/arm-compute-library_git-imx.bb:do_unpack) failed with exit code '1'

 

Can you please tell me how you resolved ?  

Thank you!

Regards, 

Rohit

0 件の賞賛
返信

10,312件の閲覧回数
q325mg
Contributor II

I have the same issue but with IMX8 QXP MEK

Were you able to fix it alexeymodyanov

Thanks

Edit:

The way it worked for was: the first time I was using Ubuntu 16, and tried to create the image on a restricted network, so I had to manually disable SSL from git and https from python, and I got the error, then instead I created a clean new Ubuntu 18 installation and did the build on a unrestricted network and it worked

0 件の賞賛
返信

9,937件の閲覧回数
luciomonteros
Contributor I

How did you disable SSL from git and https from python ?

And then you copied all the files created in tmp in ubuntu 16 to ubuntu 18 ?

タグ(1)
0 件の賞賛
返信

10,311件の閲覧回数
radhikasomaiya
Senior Contributor II


Hi  Alexey Modyanov,

We are able to build image successfully for imx6qpsabresd by following the steps of attached Yocto User's guide version L4.14.98_2.0.0. Can you please try to fresh build?

For git-lfs: not found error, you can try to install git-lfs.

Refer this link for git-lfs installation.

Regards,

Radhika Somaiya.