frequency scaling feature in IMX50

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

frequency scaling feature in IMX50

1,508 Views
lyfsci
Contributor III

Hi Experts,

Does IMX508 supports frequency scaling feature i.e changing frequency during the run time ?

In that case what is the latency in taking effect of the new frequency ?

Labels (1)
0 Kudos
Reply
1 Reply

1,369 Views
igorpadykov
NXP Employee
NXP Employee

Hi lyf

yes it supports, please refer to attached document

Chapter 10 Dynamic Voltage Frequency Scaling (DVFS) Driver.

Latency is defined by PLL lock time, described in

IMX50CEC Table 36. DPLL Electrical Parameters.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply