frequency scaling feature in IMX50

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

frequency scaling feature in IMX50

1,538件の閲覧回数
lyfsci
Contributor III

Hi Experts,

Does IMX508 supports frequency scaling feature i.e changing frequency during the run time ?

In that case what is the latency in taking effect of the new frequency ?

ラベル(1)
0 件の賞賛
返信
1 返信

1,399件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi lyf

yes it supports, please refer to attached document

Chapter 10 Dynamic Voltage Frequency Scaling (DVFS) Driver.

Latency is defined by PLL lock time, described in

IMX50CEC Table 36. DPLL Electrical Parameters.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信