freescale patch for the 2014 Uboot Android booti and fastboot command?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

freescale patch for the 2014 Uboot Android booti and fastboot command?

1,698 Views
jonathansmyth
Contributor III

hi guys,

I'm just wondering is there a patch for the 2014 uboot that incorporates the booti and fastboot commands for android

building on imx6 SOC's/

Thanks Jonny

Labels (2)
1 Reply

1,440 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Jonny,

Have you tried with the last Android BSP image from Freescale (Kitkat)? Additionally, you could take a look at the comments of the following thread:

https://community.freescale.com/message/483019

Hope this will be useful for you.
Best regards!
/Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------