freescale patch for the 2014 Uboot Android booti and fastboot command?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

freescale patch for the 2014 Uboot Android booti and fastboot command?

1,708件の閲覧回数
jonathansmyth
Contributor III

hi guys,

I'm just wondering is there a patch for the 2014 uboot that incorporates the booti and fastboot commands for android

building on imx6 SOC's/

Thanks Jonny

ラベル(2)
1 返信

1,450件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi Jonny,

Have you tried with the last Android BSP image from Freescale (Kitkat)? Additionally, you could take a look at the comments of the following thread:

https://community.freescale.com/message/483019

Hope this will be useful for you.
Best regards!
/Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------