freescale linux

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

freescale linux

1,533 次查看
sreevidyam
Contributor I

hello guys,

i am trying to work on imx31 series for ma project. can anyone say which linux os is compatible with imx31 family? and how can i get it? and also is all the linux versions compatible with all imx31 series?

标记 (1)
0 项奖励
回复
1 回复

1,263 次查看
CarlosCasillas
NXP Employee
NXP Employee

Hi,

The i.MX31 is now a legacy product and the available Linux BSP is with the kernel 2.6 on LTIB. You could also check if Timesys provides additional BSP releases at the following link:

https://linuxlink.timesys.com/dev_center/imx31

If you are start developing, it would be an option considering a newer i.MX processor, like the i.MX6 or i.MX7, which include BPSs with Linux 4.1.15 on the Yocto Project, and also Android 6.0 support:

i.MX Applications Processors|ARM® Cores|NXP

Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复