freescale imx6 How to use File Explorer in android4.3?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

freescale imx6 How to use File Explorer in android4.3?

ソリューションへジャンプ
2,125件の閲覧回数
陳冠儒
Contributor IV

hi,All:

freescale imx6 How to use File Explorer in android4.3?

After the boot,want have File Explorer.

please help me,thanks.

(中譯: 在freescale imx6 如何在android4.3上,一開機就有檔案總管?)

ラベル(4)
0 件の賞賛
返信
1 解決策
2,023件の閲覧回数
art
NXP Employee
NXP Employee

Actually, the Android BSPs by Freescale come in very "raw" state due to license limitations from Google. That's why there is no File Explorer application here. Use the Terminal application rather than the File Explorer one to install APKs.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,024件の閲覧回数
art
NXP Employee
NXP Employee

Actually, the Android BSPs by Freescale come in very "raw" state due to license limitations from Google. That's why there is no File Explorer application here. Use the Terminal application rather than the File Explorer one to install APKs.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,023件の閲覧回数
陳冠儒
Contributor IV

hi Artur Petukhov:

thank u answer,so,how I want to use the Terminal application to install the APK?

I'm sorry I'm not very familiar with android.

Please help me,thanks.

(中譯: 感謝妳的回答,原來如此,我要如何去使用 Terminal application 去安裝APK呢?

           抱歉我不是很熟android.

)

0 件の賞賛
返信
2,023件の閲覧回数
BiyongSUN
NXP Employee
NXP Employee

Mr Chen,

The question is for i.MX6 a sillicon chip or for an OS android?

I thinks if you can raise such question to android forum will be much productive.

0 件の賞賛
返信
2,023件の閲覧回数
陳冠儒
Contributor IV

Hi,Biyong Sun:

Thank u answer.
Because I think for imx6 of android4.3 BSP why not pack into the File Explorer.

So I think to ask the people here would be more clearly.

Please help me,Because I design a board to need install APK.

(中譯: 感謝妳的回答.

           因為我認為對imx6 的android4.3 BSP為何沒包入檔案總管的APP呢.

           所以我在想文這裡的人可能會比較清楚.

           請幫忙我,因為我設計一塊板子需要能自行安裝APK.

)

0 件の賞賛
返信