freescale git clone issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

freescale git clone issue

1,403 Views
pavansingpatil
Contributor I

Hi,

is there any issue with freescale git server, can't clone imx_4.9.11_1.0.0_ga kernel http://git.freescale.com/git/cgit.cgi/imx/linux-imx.git server. getting stuck for forever.

linux-imx.git - i.MX Linux Kernel 

0 Kudos
Reply
1 Reply

1,256 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Pavansingpatil,

Are you still experiencing issues cloning the git?

Would you please list the complete command you are using to try to reproduce this issue?

Some community users have reported intermittent issues with the git repositories (in rare occasions the problem may also be that a firewall is not allowing the git protocol port).

Regards,

0 Kudos
Reply