flexcan in IMX8QM MEK with base board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

flexcan in IMX8QM MEK with base board

1,186 Views
redwanmohamed
Contributor III

Hi NXP team,

Could you pls let us know how to evaluate flexcan in imx8qm mek & base board. We are running android_p9.0.0_2.1.1-auto-ga release from NXP

Is it possible to interconnect CAN0, CAN1 dump the values from the console and see it in the Android GUI. Just to see the clean communication from kernel to HAL(HIDL) to the application

Thanks

Redwan

1 Reply

1,086 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Redwan,

As a general overview the concept test application should work to validate the FlexCAN functionality.

However, I’m afraid that i.MX8QM family is still on preproduction and additional support cannot be provided yet. In case of requiring further help, please contact with your Sales/FAE.

Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
-------------------------------------------------------------------------------