file transfer via bluetooth

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

file transfer via bluetooth

ソリューションへジャンプ
3,444件の閲覧回数
fresxc
Contributor I

Hi, All

  I want to send and recive file via bluetooth between the imx6ul and iphone(or Android phone). Now, I use the rootfs from yocto project, it contains the bluez5, but there is no openobex tools. how to compile openobex tools into the rootfs in yocto project? 

Fresxc

ラベル(3)
0 件の賞賛
返信
1 解決策
3,072件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Fresxc

please refer to

OpenEmbedded Layer Index - openobex 
How to add a new layer and a new recipe in Yocto 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,073件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Fresxc

please refer to

OpenEmbedded Layer Index - openobex 
How to add a new layer and a new recipe in Yocto 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
3,073件の閲覧回数
fresxc
Contributor I

Hi igor

    I tried the way and it works. However, it only can send file from phone(Android) to imx6ul. Connect timeout when send file from imx6ul to phone.

Later, i copy the log to here. however, thanks for your reply. 

Best regards

0 件の賞賛
返信