ffmpeg only vs Gstreamer solution

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ffmpeg only vs Gstreamer solution

6,033件の閲覧回数
AdCmo
Contributor III

All,
 

Has anyone ever built a complete capture-->compress-->transmit solution on i.MX53 or similar boards?

i.e. using only ffmpeg libraries without using Gstreamer nor Gstreamer's ffmpeg plugin?

I am trying to figure out the pros and cons of using only ffmpeg and removing Gstreamer from the build tree.

Thanks,

Ad.

----------------------

ラベル(1)
タグ(2)
0 件の賞賛
返信
5 返答(返信)

3,998件の閲覧回数
Filippo
Contributor III

I'm using only ffmpeg as "local" player, the movie is on the file system. I have plans to play a network steam, in the next few days. Currently I'm using buildroot for the file system and the compiler, with an external compiled kernel ( e.g. not compiled inside the buildroot environment ).
I'm not using LTIB.
The player is ffplay from ffmpeg, so for now is a really basic application. Hope this helps.
Fil

0 件の賞賛
返信

3,998件の閲覧回数
AdCmo
Contributor III

Nice to hear. We are also working on the FFmpeg only solution and will update when done.

Can you give a usage scenario for your case?

e.g. server commands and client command setup?

Thanks,

Ad.

--------------

0 件の賞賛
返信

3,998件の閲覧回数
Filippo
Contributor III

HI,

I'm currently using only ffmplay, SDL only, no gstreamer. I'm interested in the comments about this discussion.

Fil

0 件の賞賛
返信

3,998件の閲覧回数
AdCmo
Contributor III

Daiane,

Thanks for the link. But this still uses Gstreamer for piping and all.

I wanted something more ffmpeg clean, e.g.

$ ffserver src_video dest_addr src_res out_port.

And the reciever will have something like:

$ ffplay src_video src_addr src_res in_port

Any pros and cons to this idea are welcome.

Just hoping I don't have to re-invent the wheel,

Thanks,

Ad.

------------------------------

0 件の賞賛
返信

3,998件の閲覧回数
daiane_angolini
NXP Employee
NXP Employee

>>Has anyone ever built a complete capture-->compress-->transmit solution on i.MX53 or similar boards?

http://www.imxdev.org/wiki/index.php?title=I.MX27_ADS_Board_Video_GST_Video_Streaming

0 件の賞賛
返信