fbGetDisplayByIndex() missing from libEGL.so since imx-gpu-viv-6.4.11.p2.6 (L6.6.23_2.0.0)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

fbGetDisplayByIndex() missing from libEGL.so since imx-gpu-viv-6.4.11.p2.6 (L6.6.23_2.0.0)

1,018件の閲覧回数
klarinettli
Contributor I

Since imx-gpu-viv-6.4.11.p2.6 the symbols fbGetDisplayByIndex()/fbGetDisplay()/etc. are missing from libEGL.so. The symbols are defined in gpu-core/usr/include/EGL/eglvivante.h

The configure step of qtbase uses fbGetDisplayByIndex() to determine if the vivante backend shall be compiled. The same function is also used functionally in QT.

Are theses symbols missing on purpose? If yes, in which library are they available now?

ラベル(1)
タグ(1)
0 件の賞賛
返信
3 返答(返信)

988件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hello,

Which platform are you based on? Wayland or eglfs? And can you share the error you are facing?

Best Regards,
Zhiming

0 件の賞賛
返信

978件の閲覧回数
klarinettli
Contributor I

We're using the eglfs platform.

As shown below, the "fbGetDisplayByIndex" symbol remains in the header file but is missing in the actual libraries in 6.4.11.p2.6:

❯ grep -r fbGetDisplayByIndex imx-gpu-viv-6.4.11.p2.2-aarch32-fd0148d
imx-gpu-viv-6.4.11.p2.2-aarch32-fd0148d/gpu-core/usr/include/EGL/eglvivante.h:fbGetDisplayByIndex(
grep: imx-gpu-viv-6.4.11.p2.2-aarch32-fd0148d/gpu-core/usr/lib/fb/libEGL.so.1.5.0: binary file matches
grep: imx-gpu-viv-6.4.11.p2.2-aarch32-fd0148d/gpu-core/usr/lib/fb/libVDK.so.1.2.0: binary file matches
grep: imx-gpu-viv-6.4.11.p2.2-aarch32-fd0148d/gpu-core/usr/lib/wayland/libEGL.so.1.5.0: binary file matches

❯ grep -r fbGetDisplayByIndex imx-gpu-viv-6.4.11.p2.6-aarch64-bc7b6a2
imx-gpu-viv-6.4.11.p2.6-aarch64-bc7b6a2/gpu-core/usr/include/EGL/eglvivante.h:fbGetDisplayByIndex(

 

0 件の賞賛
返信

966件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hello,

If you are using i.MX8MM, please use eglfs_kms which using drm api.

The eglfs_vivi is for i.MX6, the gpu library has removed the FB support on i.MX8

Best Regards,
Zhiming

0 件の賞賛
返信