falconboot on imx8

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

falconboot on imx8

761 次查看
KrisJ
Contributor II

Hi all, 

i am trying to enable the falcon boot mode on the imx8, i got it working on the imx6, however on the imx8evk after adding line #define CONFIG_SPL_OS_BOOT  board stops after spl doesn't boot into the uboot.

U-Boot SPL 2020.04-49995-g7ffdddacd2-dirty (Mar 30 2022 - 15:27:14 +0530)
Normal Boot
Trying to boot from BOOTROM
image offset 0x8000, pagesize 0x200, ivt offset 0x0

if i remove the line #define CONFIG_SPL_OS_BOOT from my config file i can boot the board without any problem. 

how can i make the board to load the uboot when the spl_os_boot is enabled.

Thanks,

-Krisj

0 项奖励
回复
0 回复数