failed to encode frame: failure timeout

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

failed to encode frame: failure timeout

2,601件の閲覧回数
aminebouhoula
Contributor I

Hello,

I am trying to use iMX6 to stream camera input via HDMI using gstreamer using the next command:

gst-launch-1.0 -e --gst-debug-level=2 imxv4l2src device=/dev/video0 ! imxvpuenc_h264 ! mpegtsmux ! hlssink max-files=5 target-duration=2 playlist-location=/www/pages/playlist.m3u8 location=/www/pages/segment%05d.ts playlist-length=3

After few seconds, I always get the next error:

0:00:22.326621669  1492  0x1353520 ERROR imxvpubaseenc ../src/vpu/encoder/base_enc.c:804:gst_imx_vpu_base_enc_handle_frame:<imxvpuh264enc0> failed to encode frame: failure timeout

Please help me.

Thanks a lot!

ラベル(3)
0 件の賞賛
返信
3 返答(返信)

2,279件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

what yocto version do you use? you mean that you can capture video correctly fisrt, then faile? could you upload the complete log file?

0 件の賞賛
返信

2,279件の閲覧回数
aminebouhoula
Contributor I

Thanks for your answer:

uname -a ==> Linux ventana 3.10.17-1.0.0_ga+yocto+g4d177f6

Full output:

root@ventana:~# gst-launch-1.0 -e --gst-debug-level=2 imxv4l2src device=/dev/video0 ! imxvpuenc_h264 ! mpegtsmux ! hlssink max-files=5 target-duration=2 playlist-location=/www/pages/playlist.m3u8 location=/www/pages/segment%05d.ts playlist-length=3

Setting pipeline to PAUSED ...

[INFO]  Product Info: i.MX6Q/D/S

Pipeline is live and does not need PREROLL ...

Setting pipeline to PLAYING ...

New clock: GstSystemClock

[INFO]  ringBufferEnable 0, chromaInterleave 0, mapType 0, linear2TiledEnable 0

[WARN]  VPU iram is less than needed, some parts don't use iram

0:00:54.297814674 15063  0x1d40520 ERROR          imxvpubaseenc ../src/vpu/encoder/base_enc.c:804:gst_imx_vpu_base_enc_handle_frame:<imxvpuh264enc0> failed to encode frame: failure timeout

[INFO]  vpu_SWReset

0:00:54.303632674 15063  0x1d40520 WARN                 basesrc /home/amine/ventana-yocto2/build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/gstreamer1.0/1.4.1-r0/gstreamer-1.4.1/libs/gst/base/gstbasesrc.c:2933:gst_base_src_loop:<imxv4l2src0> error: Internal data flow error.

0:00:54.305582340 15063  0x1d40520 WARN                 basesrc /home/amine/ventana-yocto2/build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/gstreamer1.0/1.4.1-r0/gstreamer-1.4.1/libs/gst/base/gstbasesrc.c:2933:gst_base_src_loop:<imxv4l2src0> error: streaming task paused, reason error (-5)

ERROR: from element /GstPipeline:pipeline0/GstImxV4l2Src:imxv4l2src0: Internal data flow error.

Additional debug info:

/home/amine/ventana-yocto2/build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/gstreamer1.0/1.4.1-r0/gstreamer-1.4.1/libs/gst/base/gstbasesrc.c(2933): gst_base_src_loop (): /GstPipeline:pipeline0/GstImxV4l2Src:imxv4l2src0:

streaming task paused, reason error (-5)

EOS on shutdown enabled -- waiting for EOS after Error

Waiting for EOS...

Got EOS from element "pipeline0".

EOS received - stopping pipeline...

Execution ended after 0:00:54.009322674

Setting pipeline to PAUSED ...

Setting pipeline to READY ...

Setting pipeline to NULL ...

Freeing pipeline ...

0 件の賞賛
返信

2,279件の閲覧回数
aminebouhoula
Contributor I

Any help please?

0 件の賞賛
返信