failed to bitbake tensorflow-lite

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

failed to bitbake tensorflow-lite

2,117 Views
jimmyli
Contributor V

Hi 

      I am downloading the L5.10.9_1.0.0 linux source code for i.mx8m plus by yocto, now I encounter a problem showed as below.

      Hope you can help me.

      Thanks.

//////////////////////////////////////

Build Configuration:
BB_VERSION = "1.48.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "ubuntu-20.04"
TARGET_SYS = "aarch64-poky-linux"
MACHINE = "imx8mpevk"
DISTRO = "fsl-imx-wayland"
DISTRO_VERSION = "5.10-gatesgarth"
TUNE_FEATURES = "aarch64 armv8a crc cortexa53 crypto"
TARGET_FPU = ""

...

 

ERROR: tensorflow-lite-2.4.0-r0 do_configure: Execution of '/home/jimmy/yocto/imx8mp-yocto-bsp/build-wayland/tmp/work/cortexa53-crypto-poky-linux/tensorflow-lite/2.4.0-r0/temp/run.do_configure.3893655' failed with exit code 4:
downloading https://gitlab.com/libeigen/eigen/-/archive/011e0db31d1bed8b7f73662be6d57d9f30fa457a/eigen-011e0db31...
--2021-05-31 10:54:41-- https://gitlab.com/libeigen/eigen/-/archive/011e0db31d1bed8b7f73662be6d57d9f30fa457a/eigen-011e0db31...
Resolving gitlab.com (gitlab.com)... 2606:4700:90:0:f22e:fbec:5bed:a9b9, 172.65.251.78
Connecting to gitlab.com (gitlab.com)|2606:4700:90:0:f22e:fbec:5bed:a9b9|:443... failed: Connection timed out.
Connecting to gitlab.com (gitlab.com)|172.65.251.78|:443... connected.
Unable to establish SSL connection.
WARNING: exit code 4 from a shell command.

ERROR: Logfile of failure stored in: /home/jimmy/yocto/imx8mp-yocto-bsp/build-wayland/tmp/work/cortexa53-crypto-poky-linux/tensorflow-lite/2.4.0-r0/temp/log.do_configure.3893655

 

 

Labels (1)
0 Kudos
Reply
1 Reply

2,113 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello jimmyli,

 

Apparently you have problem with your network since yocto bsp build all rigth.

Regards

 

0 Kudos
Reply