failed during write leveling calibration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

failed during write leveling calibration

4,287 Views
vinothkumars
Senior Contributor IV

Hi All,

   I am testing a new hardware using i.MX6 solo interfaced with DDR3 by running DDR stress test v2.60 tool and it's failed during calibration and I got error.

Please see debug message as following:

Normal Boot
Hit any key to stop autoboot:  0
=> dcache off
=> icache off
=> ext4load mmc 0:1 0x907000 ddr-test-uboot-jtag-mx6dl.bin
71812 bytes read in 127 ms (551.8 KiB/s)
=> go 0x907000
## Starting application at 0x00907000 ...

============================================
        DDR Stress Test (3.0.0)
        Build: Dec 14 2018, 14:20:16
        NXP Semiconductors.
============================================

============================================
        Chip ID
CHIP ID = i.MX6 Solo/DualLite (0x61)
Internal Revision = TO1.3
============================================

============================================
        Boot Configuration
SRC_SBMR1(0x020d8004) = 0x00000040
SRC_SBMR2(0x020d801c) = 0x22000001
============================================

What ARM core speed would you like to run?
Type 1 for 800MHz, 2 for 1GHz
ARM Clock set to 800MHz

============================================
        DDR configuration
BOOT_CFG3[5-4]: 0x00, Single DDR channel.
DDR type is DDR3
Data width: 32, bank num: 8
Row size: 15, col size: 10
Chip select CSD0 is used
Density per chip select: 1024MB
============================================

Current Temperature: 45
============================================

Please select the DDR density per chip select (in bytes) on the board
Type 0 for 2GB; 1 for 1GB; 2 for 512MB; 3 for 256MB; 4 for 128MB; 5 for 64MB; 6 for 32MB  
For maximum supported density (4GB), we can only access up to 3.75GB.  Type 7 to select this
  DDR density selected (MB): 1024


Would do you want to change VDD_SOC_CAP/VDD_ARM_CAP voltage? Type 'y' to run and 'n' to skip


Would do you want run DDR Calibration? Type 'y' to run and 'n' to skip

Calibration will run at DDR frequency 400MHz. Type 'y' to continue.
If you want to run at other DDR frequency. Type 'n'
  Please enter the MR1 value on the initilization script
  This will be re-programmed into MR1 after write leveling calibration
  Enter as a 4-digit HEX value, example 0004, then hit enter
0004DDR Freq: 396 MHz

ddr_mr1=0x00000004
Start write leveling calibration...
running Write level HW calibration
  MPWLHWERR register read out for factory diagnostics:
  MPWLHWERR PHY0 = 0x00000000


HW WL cal status: no suitable delay value found for byte 0

HW WL cal status: no suitable delay value found for byte 1

HW WL cal status: no suitable delay value found for byte 2

HW WL cal status: no suitable delay value found for byte 3
Write leveling calibration completed but failed, the following results were found:
    MMDC_MPWLDECTRL0 ch0 (0x021b080c) = 0x001F001F
    MMDC_MPWLDECTRL1 ch0 (0x021b0810) = 0x001F001F
Write DQS delay result:
   Write DQS0 delay: 31/256 CK
   Write DQS1 delay: 31/256 CK
   Write DQS2 delay: 31/256 CK
   Write DQS3 delay: 31/256 CK


Error: failed during write leveling calibration

Regards,

VinothS

Regards,
Vinothkumar Sekar
Labels (3)
0 Kudos
Reply
3 Replies

3,846 Views
vinothkumars
Senior Contributor IV

DDR Calibration done by old version of tools. I closed this thread now.

DDR_Stress_Tester_V1.0.3_UART1_for_Sdboot&JTAG.zip

Regards,

VinothS

Regards,
Vinothkumar Sekar
0 Kudos
Reply

3,846 Views
igorpadykov
NXP Employee
NXP Employee

Hi Vinoth

write leveling calibration can complete even processor ddr interface and memory

connections are not configured properly.

One can recheck ddr memory connections using i.MX6 System Development User’s Guide

and check with oscilloscope ddr signals performing memory accesses with jtag.

https://www.nxp.com/docs/en/user-guide/IMX6DQ6SDLHDG.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

3,846 Views
vinothkumars
Senior Contributor IV

Hi Igor,

DDR Calibration was done using older version (DDR_Stress_Tester_V1.0.3_UART1) instead of 3.0.1.

And now I got some other problem.

For every board I got some different value and also I got following error in one of my board,

[Mon Feb 18 14:12:47.175 2019] ERROR FOUND, we can't get suitable value !!!!
[Mon Feb 18 14:12:47.175 2019] dram test fails for all values. 

Thanks & Regards,

VinothS

Regards,
Vinothkumar Sekar
0 Kudos
Reply