facing an error while flashing android9.0 images in a imx6 board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

facing an error while flashing android9.0 images in a imx6 board

2,756 Views
shilesh_babu
Contributor II

Hi All,

Can anyone help why I am facing below issue, while flashing the images in the Toradex apalis imx6 board?

Device-Info:-

Device: FSL_SDHC
Manufacturer ID: 13
OEM: 14e
Name: Q2J54
Tran Speed: 52000000
Rd Block Len: 512
MMC version 5.0
High Capacity: Yes
Capacity: 3.6 GiB
Bus Width: 8-bit
Erase Group Size: 512 KiB
HC WP Group Size: 8 MiB
User Capacity: 3.6 GiB WRREL
Boot Capacity: 2 MiB ENH
RPMB Capacity: 512 KiB ENH

Flashing-Steps:-

.\uuu_imx_android_flash.bat -f imx6q -p sabrsd -e

error:

1:2      1/22 [                                      ] FB: ucmd setenv fastboot_dev mmc                                               
Success 0    Failure 1                                                                    

Thank you!!

Labels (2)
Tags (1)
0 Kudos
Reply
4 Replies

2,658 Views
igorpadykov
NXP Employee
NXP Employee

Hi shilesh

one can try to follow sect.5 Programming Images attached Android_User's_Guide.pdf

more documentation can be found on i.MX Software and Development Tools | NXP 

Also may be useful to post issue on toradex forum :

problem installing android in my toradex apalis imx6 - Toradex Community 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,658 Views
shilesh_babu
Contributor II

Hi Igor,

I have a doubt, my imx6 apalis board have only Capacity: 3.6 GB emmc, is this possible to flash android9.0 images because google Android 9 Compatibility documents have mentioned /data partition size must be greater then 4GB.

Android 9 Compatibility Definition  |  Android Open Source Project

[7.6.1/H-10-1] MUST have at least 4GB of non-volatile storage available for application private data (a.k.a. "/data" partition).

Thank you!!

0 Kudos
Reply

2,658 Views
shilesh_babu
Contributor II

Thanks for your reply @igor,

0 Kudos
Reply

2,658 Views
shilesh_babu
Contributor II

Is this emmc issue?

0 Kudos
Reply