f_stat function doesn't seem to work

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

f_stat function doesn't seem to work

1,394 Views
ranjay_shandilya
Contributor III

Hi,

I'm trying to use fatfs with freertos and f_stat call is returning FR_NO_PATH even though path is correct.

/*Code*/

bool IFileSystem::FileExists(const GCPString &Filename, const bool bSecureCheck /* = false */)
{
PRINTF("IFileSystem::FileExists >>>> Filename = %s\r\n",Filename.c_str());
bool rv = false;
#ifdef GCPOS_FREERTOS
FRESULT fr;
FILINFO fno;
fr = f_stat(Filename.c_str(), &fno);
switch (fr) {

case FR_OK:
rv = true;
break;

case FR_NO_FILE:
rv = false;
break;

default:
rv = false;
PRINTF("IFileSystem::FileExists default case FR_NO_FILE = (%d)\r\n",(int)fr);
}
return rv;

*/Code 

Filepath :  "./hon/data/Panel.sqlite";

Can someone pls help? 

Board:iMXRT1050EVKB

 

Thanks

0 Kudos
Reply
1 Reply

1,382 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello
Hope you are well.
It will be helpful to check an SDK example as a reference. When passing the file path parameter the examples use _T("filepaht").
It could also be helpful if you share more details about your project so I can reproduce this issue.

If you have more questions do not hesitate to ask me.
Best regards,
Omar

0 Kudos
Reply