ethernet switch

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ethernet switch

3,349件の閲覧回数
Seattle_EE
Contributor I

What are people using to connect multiple ethernet ports to the i.MX6?  I am having a difficult time finding a suitable 3-port, tri-mode ethernet switch.  We wish to connect two devices with the CPU, so two PHY and one RGMII to the i.MX6.  Plenty of 10/100 solutions, but am having difficulty finding 10/100/1000.

Thanks.

ラベル(6)
0 件の賞賛
返信
5 返答(返信)

2,829件の閲覧回数
rohitarora
Contributor I

Craig you can go with 88E6350

0 件の賞賛
返信

2,829件の閲覧回数
YixingKong
Senior Contributor IV

Craig

This discussion is closed since no activity. If you still need help, please feel free to reply with an update to this discussion, or create another discussion.

Thanks,

Yixing

0 件の賞賛
返信

2,829件の閲覧回数
drummer
Contributor IV

I am using KSZ8873MLL.

0 件の賞賛
返信

2,829件の閲覧回数
Seattle_EE
Contributor I

The only problem with that switch is that it is only for 10/100.  I need GbE.

0 件の賞賛
返信

2,829件の閲覧回数
YixingKong
Senior Contributor IV

Craig


We are sorry for getting back to you so late. Are you still stuck with the issue? If you have somehow to resolved the issue, can we close the discussion? If you still need help, please feel free to reply with an update to this discussion.

Thanks,
Yixing

0 件の賞賛
返信