ethernet: Varying network bandwith @TCP/IP stack level

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ethernet: Varying network bandwith @TCP/IP stack level

1,236件の閲覧回数
shajinas
Contributor I

Hello all,

I am working on a custom platform based on i.MX6Q Sabresd SD. The software running on the platform is Yocto BSP kernel version 3.14.28 from Freescale.

The custom platform has an on board ethernet controller which is connected to i.MX6Q via local bus(EIM) and we were  able to establish network connectivity.

I would like to understand on how to vary the network bandwidth at TCP/IP stack level inside kernel. Say for example, I would like to  vary the link bandwidth from Gigabit to 10Mbpps Half/Full Duplex. Many people used ethtool to vary the bandwidth, However it hides the kernel internals.

Any pointers on how to vary the bandwidth @ TCP/IP level would be appreciated.

Thanks

Shajin

ラベル(5)
0 件の賞賛
返信
1 返信

1,187件の閲覧回数
b36401
NXP Employee
NXP Employee

There is nothing special to i.MX.

You can limit network bandwidth using Linux "tc" utility.

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信