I am trying to get an ipv4 and ipv6 address on eth0. Our board is based on imx28evk, but has only eth0 (no eth1).
My question is what configuration am I missing in the yocto build that eth0 does not get both ipv4 and ipv6 addresses ?
In the absence of an IPV6 dhcp server, I thought eth0 would get alteast a link local ipv6 address ?
Here is my configuration:
/etc/network/interfaces:
# /etc/network/interfaces -- configuration file for ifup(8), ifdown(8)
# The loopback interface
auto lo
iface lo inet loopback
# Wired or wireless interfaces
auto eth0
iface eth0 inet dhcp
hwaddress ether 00:04:0F:03:52:02
pre-up ifconfig $IFACE up
post-down IFCONDIG $IFACE down
iface eth0 inet6 manual
pre-up ifconfig $IFACE up
post-down ifconfig $IFACE down
hwaddress ether 00:04:0F:03:52:02
avahi-autoipd kicks in when there is no dhcp. When there is no ipv4 dhcp server, ifconfig gives me:
root@imx28evk:~# ifconfig
eth0 Link encap:Ethernet HWaddr 00:04:0F:03:52:02
UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:57 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:11600 (11.3 KiB)
Base address:0x8000
eth0:avahi Link encap:Ethernet HWaddr 00:04:0F:03:52:02
inet addr:169.254.154.166 Bcast:169.254.255.255 Mask:255.255.0.0
UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1
Base address:0x8000
lo Link encap:Local Loopback
inet addr:127.0.0.1 Mask:255.0.0.0
inet6 addr: ::1/128 Scope:Host
UP LOOPBACK RUNNING MTU:16436 Metric:1
RX packets:126 errors:0 dropped:0 overruns:0 frame:0
TX packets:126 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:0
RX bytes:9240 (9.0 KiB) TX bytes:9240 (9.0 KiB)
sysctl does not have eth0 related keys. It does have keys for l0 and eth1. Trying to enable ipv6 for eth0 gives me an "sysctl error: unknown keys.
net.ipv6.conf.all.forwarding = 0
net.ipv6.conf.all.hop_limit = 64
net.ipv6.conf.all.mtu = 1280
net.ipv6.conf.all.accept_ra = 1
net.ipv6.conf.all.accept_redirects = 1
net.ipv6.conf.all.autoconf = 1
net.ipv6.conf.all.dad_transmits = 1
net.ipv6.conf.all.router_solicitations = 3
net.ipv6.conf.all.router_solicitation_interval = 4
net.ipv6.conf.all.router_solicitation_delay = 1
net.ipv6.conf.all.force_mld_version = 0
net.ipv6.conf.all.max_addresses = 16
net.ipv6.conf.all.accept_ra_defrtr = 1
net.ipv6.conf.all.accept_ra_pinfo = 1
net.ipv6.conf.all.proxy_ndp = 0
net.ipv6.conf.all.accept_source_route = 0
net.ipv6.conf.all.disable_ipv6 = 0
net.ipv6.conf.all.accept_dad = 1
net.ipv6.conf.all.force_tllao = 0
net.ipv6.conf.default.forwarding = 0
net.ipv6.conf.default.hop_limit = 64
net.ipv6.conf.default.mtu = 1280
net.ipv6.conf.default.accept_ra = 1
net.ipv6.conf.default.accept_redirects = 1
net.ipv6.conf.default.autoconf = 1
net.ipv6.conf.default.dad_transmits = 1
net.ipv6.conf.default.router_solicitations = 3
net.ipv6.conf.default.router_solicitation_interval = 4
net.ipv6.conf.default.router_solicitation_delay = 1
net.ipv6.conf.default.force_mld_version = 0
net.ipv6.conf.default.max_addresses = 16
net.ipv6.conf.default.accept_ra_defrtr = 1
net.ipv6.conf.default.accept_ra_pinfo = 1
net.ipv6.conf.default.proxy_ndp = 0
net.ipv6.conf.default.accept_source_route = 0
net.ipv6.conf.default.disable_ipv6 = 0
net.ipv6.conf.default.accept_dad = 1
net.ipv6.conf.default.force_tllao = 0
net.ipv6.conf.lo.forwarding = 0
net.ipv6.conf.lo.hop_limit = 64
net.ipv6.conf.lo.mtu = 16436
net.ipv6.conf.lo.accept_ra = 1
net.ipv6.conf.lo.accept_redirects = 1
net.ipv6.conf.lo.autoconf = 1
net.ipv6.conf.lo.dad_transmits = 1
net.ipv6.conf.lo.router_solicitations = 3
net.ipv6.conf.lo.router_solicitation_interval = 4
net.ipv6.conf.lo.router_solicitation_delay = 1
net.ipv6.conf.lo.force_mld_version = 0
net.ipv6.conf.lo.max_addresses = 16
net.ipv6.conf.lo.accept_ra_defrtr = 1
net.ipv6.conf.lo.accept_ra_pinfo = 1
net.ipv6.conf.lo.proxy_ndp = 0
net.ipv6.conf.lo.accept_source_route = 0
net.ipv6.conf.lo.disable_ipv6 = 0
net.ipv6.conf.lo.accept_dad = -1
net.ipv6.conf.lo.force_tllao = 0
net.ipv6.conf.eth1.forwarding = 0
net.ipv6.conf.eth1.hop_limit = 64
net.ipv6.conf.eth1.mtu = 1500
net.ipv6.conf.eth1.accept_ra = 1
net.ipv6.conf.eth1.accept_redirects = 1
net.ipv6.conf.eth1.autoconf = 1
net.ipv6.conf.eth1.dad_transmits = 1
net.ipv6.conf.eth1.router_solicitations = 3
net.ipv6.conf.eth1.router_solicitation_interval = 4
net.ipv6.conf.eth1.router_solicitation_delay = 1
net.ipv6.conf.eth1.force_mld_version = 0
net.ipv6.conf.eth1.max_addresses = 16
net.ipv6.conf.eth1.accept_ra_defrtr = 1
net.ipv6.conf.eth1.accept_ra_pinfo = 1
net.ipv6.conf.eth1.proxy_ndp = 0
net.ipv6.conf.eth1.accept_source_route = 0
net.ipv6.conf.eth1.disable_ipv6 = 0
net.ipv6.conf.eth1.accept_dad = 1
net.ipv6.conf.eth1.force_tllao = 0
if_net6 has only lo.
root@imx28evk:/proc# cat /proc/net/if_inet6
00000000000000000000000000000001 01 80 10 80 lo
Avahi assigns an ipv6 address to eth0 only if "face eth0 inet dhcp" is not commented in /etc/network/interfaces.
avahi-daemon.conf has
under [server]:
use-ipv4=yes
use-ipv6=yes
allow-interfaces=eth0
#deny-interfaces=eth1
and under [publish]
publish-aaaa-on-ipv4=yes
publish-a-on-ipv6=yes
Thanks,
Aparna