endpoint in gadgetFS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

endpoint in gadgetFS

1,333 Views
vyasvenkat1996
Contributor I

As I working on imxull board I facing Problem that I not getting the endpoints in gadgetFS.

After mounting and enable the gadgetfs on imx6ull board , I am unable to get the endpoints to setup the communication.
This are the following steps I do , Kindly provide me proper steps to get the endpoints.

root@imx6ull14x14evk:~# cd /dev/gadget/

root@imx6ull14x14evk:/dev/gadget# ls

2184000.usb

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,260 Views
igorpadykov
NXP Employee
NXP Employee

Hi venkat

one cal look at usb examples provided in

SDK2.2_iMX6ULL_WIN

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply